It looks like you are coming from United States, but the current site you have selected to visit is Israel. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Flygt Experior Pump System in Jefferson Parish

USA

Jefferson Parish sewer rates are among the lowest in the country for a system of this size and economic importance to the region. Even routine storms can spawn enough rainfall to induce surges of inflow and infiltration (I&I) that can overload stretches of the Parish’s 1500 miles of gravity sewer lines, 200 miles of force mains and 505 lift stations that range from single-horsepower installations to facilities with multiple 400-hp pumps. The Experior solution has provided Jefferson Parish 50% savings in energy costs as well as maintenance costs savings and supports the Parish’s ability to better serve the community with a reliable sewer system. Download to read the whole story.

Download Case study