It looks like you are coming from United States, but the current site you have selected to visit is Israel. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Combined sewage and stormwater pump station

USA

Challenge
To develop a combined stormwater and sewage pump station at the lowest possible cost.

Solution
The station was designed with three Flygt CP 3501 and six Flygt PL 7121 pumps. The use of a Flygt Formed Suction Intake device reduced the pump station footprint by nearly 60% and lowered the construction costs by more than 10%. This ensures reliable pumping using the smallest possible footprint.