It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Cooling water for gas-fired power plant

SWEDEN

Challenge
A gas-fired power plant in southern Sweden required a supply of cooling water to be pumped through a long pipe, which is sensitive to water hammer, to heat exchangers that are sensitive to rapid changes in pressure.

Solution
Due to a low lift system, Flygt propeller pumps are used to deliver approximately 6 m³/s (95,000 US gpm). The propeller pumps transport seawater, which is used as cooling water, into a surge tower in order to pressurize the pipeline. The surge tower guarantees that no rapid changes in pressure will occur in the pipe system, thereby preventing water hammer.