It looks like you are coming from United States, but the current site you have selected to visit is Hong Kong SAR China. Do you want to change site?

Yes, please! No, keep me on the current site

Montana water utility detects leaks faster with Sensus smart utility network

Montana water utility detects leaks faster with Sensus smart utility network

Near-real-time data helped the utility stop a 170-gallons-per-hour leak in one home within hours.

In the mountain community of Big Sky, Montana, monitoring water systems can be challenging with the large seasonal population, extreme weather and elevation changes. Leaks and other issues may occur when no one is there to notice. To help solve the problem, Big Sky Water & Sewer District deployed a smart utility network from Xylem’s Sensus brand. The network helps the utility detect leaks faster and quickly respond to customer needs.

Big Sky attracts skiers, mountain bikers and nature lovers to the Rocky Mountains. The gateway community to Yellowstone National Park has become a hot spot for seasonal residents and visitors who come from all over the country for breathtaking views and an abundance of outdoor recreation.

“As the community water utility, we’re probably the closest thing there is to a town government here,” said Big Sky Water & Sewer District General Manager Ron Edwards. “We might be a small community, but that doesn’t mean we’re not expected to provide service worthy of the name Big Sky.”

Big Sky Water & Sewer District aims to deliver a five-star experience for their 2,800 customers on par with any major resort town in the country. Their drive for excellence and enthusiasm for innovative technology puts them well on their way.

Deploying a smart utility network from Sensus

In addition to the challenges of the seasonal population and weather, the District also bills quarterly, which makes finding leaks early on even more critical for customers.

“Costs can really add up if a leak goes undetected for long,” said Edwards. “We need to be able to identify these types of things before they become big problems for customers or lead to non-revenue water issues.”

Edwards and his staff envisioned a virtual metering program that would allow the utility to aggregate meter data and better pinpoint where water is flowing. The utility deployed a smart utility network from Sensus, a Xylem brand, to provide remote system monitoring that yields advanced leak detection and quick response to customer needs.

Detecting a 170-gallons-per-hour leak at one home

Big Sky’s technology investment combined Sensus iPERL® residential water meters with the two-way FlexNet® communication network and Sensus Analytics to bring in reliable, near-real-time data from across their service area. The system promptly validated its potential when it helped technicians spot a pumped sewer service line backup that caused a 170-gallons-per-hour leak at one home.

“We connected with the customer and resolved the issue within a day,” said Edwards. “Of course the homeowner was thankful to avoid the cost and potential damage that could have come with a prolonged leak.”

In another instance, the team detected when underground lines froze beneath a condominium, a frequent occurrence in this renowned ski resort town. They had to wait until spring to fix the service line and instructed the homeowner to allow a trickle of water from one sink.

“We dispatched technicians with steam machines to help thaw the pipes before the situation could escalate,” said Edwards. “Without our network, we would not have had the information to respond so proactively or adjust the water bill accurately.”

Monitoring water pressure to detect leaks

Elevation helps form quality ski slopes in Big Sky, but it also makes monitoring water pressure important as flow moves from high to low altitude. As an extension of their technology-driven system, the utility deployed the Sensus® Smart Gateway Sensor Interface to monitor distribution across the District’s ten pressure reducing valve (PRV) sites. The battery-powered Smart Gateway is a FlexNet-enabled device that connects to a variety of applications in locations where no power or land-based communications are available.

“We’ve installed the gateway devices at three sites so far and are already experiencing benefits,” said Edwards. “The ability to see the volume of water coming through these sites allows us to better understand where we may have service area leaks.”

The Sensus network and software also allows the District to virtually group meters and quickly see daily water demand below the PRV vaults. The difference between the PRV meter flow against the virtual meter for the service area gives them the ability to narrow leak detection efforts.

Big Sky Water & Sewer District understands the role they play in preserving resources as a utility governed by Western water rights law. Edwards said their smart infrastructure is a major asset to improve water loss reduction.

“One day we’ll be able to adjust the pressure so it’s not as high during non-peak nighttime hours,” said Edwards. “Having the right technology allows us to add these types of applications, which will only increase our level of control down the road.”

Forecasting with data

Big Sky’s team now has a virtual database to collect and organize the network data. The information helps them counsel their customers.

“We have irrigation customers and hotels that are itching for insights,” said Edwards. “We can run the analysis for them right down to their hourly usage so they can get smarter with their own water goals.”

Whether the District is overseeing meter data or consulting with customers, the technology investment will continue to be instrumental in their smart water journey.

“We call the Xylem system our Swiss Army knife,” said Edwards. “It gives us a full range of tools with many purposes to help us best serve our customers.”

Learn more about how Xylem helps communities use water more sustainably in the latest Sustainability Report.