It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

潜水式柱塞泵

本部分将介绍Flygt的潜水式柱塞泵产品和我们的传统柱塞泵。所有柱塞泵都位于排放柱内,排放柱通常从顶部结构悬吊而下。潜水式柱塞泵位于排放柱底部,无需任何紧固件或特殊硬件。潜水式柱塞泵可以快速安装和拆卸,以便进行检查和维修。传统设计既可以作为现场安装的完整单元构建,也可作为拉出式设计,可将整个旋转组件从柱形管中拉出以便进行维修。

需要帮助吗?

联系专家

Contact an Expert

Whether you would like additional information or are interested in getting a quote, we're here to help.

All fields required.

*  必填字段
Product Models 技术 案例研究 & 和白皮书
Product Models
没有结果与您的搜索匹配
技术

FLYGT柱塞泵

Flygt柱塞泵是高排放流量和低等到中等扬程应用的佼佼者。该泵对于其可以处理的流量范围来说,是最具成本效益的泵型。该泵由具有固定叶片角度的旋桨或具有满足规定工况的切割量(直径)的半轴叶轮组成。

柱塞泵为高比转速泵,因此依赖于其精心设计的泵坑提供其工厂性能。Flygt拥有丰富的知识、工具和经验,可帮助您设计出良好的湿井和实用的功能泵站。

案例研究 & 和白皮书

Creating a white-water ride

SPAIN

Challenge Creating an artificial white water channel for water sports such as kayaking, canoeing and rafting by pumping 3 m3/s (48,000 US gpm) per pump at a height of 7 m (24 ft). Solution The...

阅读更多内容

Cost-efficient pump station

BELGIUM

Challenge To provide a cost-efficient pump station fed by three independent inlets, resulting in a potential maximum inflow of 7.8 m3/s (123,000 US gpm) combined. Air entrainment into the pumps due...

阅读更多内容

Propeller pump stations

MEXICO

Challenge A major city in Mexico has three different propeller pump stations to handle combined wastewater and stormwater pumping. For nine months of the year, the stations transport wastewater and...

阅读更多内容

Compact stormwater pump station

USA

Challenge Placement of a new stormwater pump station in a 10 m x 5 m (32 × 18 ft) area between two roads and a hotel in one mid-western state’s major cities. Close proximity to three rivers, snow...

阅读更多内容