It looks like you are coming from United States, but the current site you have selected to visit is Denmark. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Tillad høj kontrasttilstand

Flygt pumper med kanalpumpehjul

C-3000

PUMPER MED KANALPUMPEHJUL

  • Fås med en enkelt skovl eller flere skovle
  • Traditionelt design med stort gennemløb
  • Højt effektivitet for rent vand
  • Støbejern og valgfri pumpehjulsmaterialer

Har du brug for hjælp?

Kontakt en ekspert

Anmod om oplysninger

Uanset om du ønsker yderligere information eller er interesseret i at få et tilbud, er vi klar til at hjælpe dig.

All fields required.

*  Obligatorisk felt
Pumpemodeller Teknologi Kundehistorier & White Papers
Pumpemodeller
Ingen resultater matcher din søgning
Teknologi

FLYGT PUMPER MED KANALPUMPEHJUL

Flygt C-pumperne med kanalpumpehjul er bygget til at kunne håndtere volumener på op til 3.000 l/s med motorer på op til 775 kW.

Basisversionerne af disse pumper er fremstillet af slidstærkt støbejern, og de er beregnet til krævende applikationer, såsom kommunale spildevandssystemer og spildevand fra industrien. Eksplosionssikre versioner er tilgængelige. De klassiske C-pumper med indkapslet pumpehjul med en enkelt skovl eller flere skovle har bevist deres driftssikkerhed igennem årene.

De mindre C-pumper er udstyret med Flygt Nevaclog®-pumpehjul, som har gode egenskaber mht. passage af faste partikler. De større pumper er udstyret med pumpehjul med flere skovle, der giver maksimal hydraulisk effektivitet.

Kundehistorier & White Papers

Circular stormwater pump station

FRANCE

Challenge One of the largest airports serving France required a stormwater treatment plant to handle the inflow from a large gravity sewer collecting water from the runways. Solution The pump station...

Læs mere

Pump station with cleaning function

SWEDEN

Challenge Eighteen Flygt pump stations transport wastewater at a popular recreational and amusement area in central Stockholm. One of the pump stations handles restaurant wastewater containing fats,...

Læs mere

Expansion of a desalination plant

AUSTRALIA

Challenge One of Australia’s largest cities was running short of fresh water and needed a major expansion of its desalination facility. One hurdle was to transfer the seawater to the plant. A new...

Læs mere

Sewage and stormwater pump stations

UK

Storm water pump station design Challenge The revival of one of Britain’s largest commercially unexploited land areas called for multi-phase construction of two large pump stations. One pump station...

Læs mere

Large capacity circular wet well

USA

Challenge Very deep, large capacity and limited footprint: these are common demands by customers for their pump stations designs. Recently, two such pump stations were needed in the US. Solution The...

Læs mere

Circular wastewater lift station

USA

Challenge A 54,000-acre service area in a major city in Texas required assistance to handle a projected 50% increase in population and subsequent increase in wastewater processing demands. Solution...

Læs mere