It looks like you are coming from United States, but the current site you have selected to visit is Canada. Do you want to change sites?

Yes, please. No. Keep me on the current site.

See All Disinfectants

Chemflex™ Disinfecting Wipes Single Canister with Refills

Unit of Measure #: EA
  • is the minimum order quantity for this product. Please check quantity and add to cart again.

Request a Proposal

*  Required Field

CHEMFLEX™ Refillable Dry Wipe System has been validated with peracetic acid solutions*, citric acid and bleach (1% and 10% concentrations). The wipe material is cellulose free and will not compromise the strength of the disinfectant like some cellulose-based (paper) products.

Once a disinfectant is added to the CHEMFLEX™ System, it remains stable for five days. The refillable, closed container provides an easy, accessible method to disinfect patient areas with less exposure to vapors and reduced risk of spills.

*Reference the defined approved uses per label of disinfectant

1 canister with 150 wipes and 5 refill roles with 150 wipes each - a total of 900 wipes

  • Closed container system
  • Reduces the risk of cross contamination
  • Less exposure to vapors
  • Cellulose and latex free
  • Convenient pop-up container
  • Low lint, large (7x10”) and durable wipe material

Validation studies have been completed on PAA solutions. These studies examined the saturation levels, wipe integrity and chemical concentration over a 14-day period. Once a disinfectant is added to the CHEMFLEX™ System, it remains stable for five days. No testing is required during this time. Between days 6 and 14 you must test the disinfectant concentration daily using a test strip to ensure the disinfectant strength. Your peracetic acid supplier should supply corresponding test strips for daily validation.

When using the dry wipes for the first time, write the name of the disinfectant used on the outside of the canister. When replacing dry wipes, refill using the same disinfectant indicated on the outside of the canister.

NEVER PLACE A DIFFERENT TYPE OF DISINFECTANT IN THE CANISTER OTHER THAN WHAT IS INDICATED IN THE CHEMICAL FIELD ON THE OUTSIDE OF THE CANISTER.

CHEMFLEX Refillable Dry Wipe System requires the operator to wear personal protective equipment (PPE) as defined in the labeling of the disinfectant used with the CHEMFLEX System.