您似乎来自United States,但您选择访问的当前网站是China。是否更换网站?

是,请更换! 否,停在当前网站。

Enable high contrast mode

Successful Trials with Flygt Adaptive Mixing Technology

Challenge

Albion completed the update of several components of its four-MGD plant in the fall 2017. Afterwards, plant superintendent Kent Phillips became interested in testing the impact that optimizing his mixing might have on other aspects of his conventional activated sludge process with enhanced biological phosphorus removal.

Solution

The 4220 comes in 1.5-, 2-, 3-, and 4-horsepower models. A four-horsepower mixer can operate at any lower power level and perform with the same high efficiency as a lower power model. The old mixer was drawing 1.3kW. In the end, Phillips found he could turn the 4220 all the way down to 0.1 kW–eight percent of what the old mixer used–and still have satisfactory mixing.