It looks like you are coming from United States, but the current site you have selected to visit is United Kingdom. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Lowara gets Presidential treatment in ‘The Land of Fire’

Baku Park

Baku, Azerbaijan

Xylem Lowara in Baku

The Flame Fountain, Baku Park, Baku, 

Azerbaijan has long been called ‘The Land of Fire’ due to the visually stunning natural gas fires which blaze continuously on the hillside of the Absheron Peninsula.This has proved to be the inspiration behind the Flame Fountain sculpture which resembles a vast flame bursting from the Earth’s surface.

The Flame Fountain stands 30 m tall and forms the center piece of a new public park recently built as part of a regeneration project in the area on the Hedar Aliyev Avenue, the main highway leading into the city.

The triple helix shaped monument is equipped with over 700 banks of LED lights, 1,600 m of glass rod cladding rails and stands imposingly in the middle of a large fountain pool, transforming the skyline into a spectacular water, light and sound show.

Reaching new heights
During the stunning display, thousands of gallons of water is pumped continuously throughout the fountain pool at a maximum capacity of 1400 m3/h, at some points reaching as high as 37 m into the air.

With a monument of this stature the Flame Fountain is set to become a landmark within the capital city. It was imperative that the pumps used were reliable, could deliver water at the necessary force required while at the same time being capable of distributing thousands of gallons of water each day for the water display.

“Water forms an integral part of the monument as a whole. If this is not transferred correctly, we have no display.”
The specifiers decided to invest in market leading single stage hydraulic pumps which could pump large volumes of water both sufficiently and cost effectively.

A market leading solution
Expert installer Luca Soffritti owner of Neon Alpina Fontane was instructed to find an ideal solution to the specifier’s  equirements.
Having worked with Lowara’s portfolio of high quality products for a number of years, Luca Soffritti was quick to explain the benefits of the new range of end suction centrifugal pumps – ideal for the Flame Fountain display.

During the water display there are in total 26 Lowara end suction centrifugal pumps, which transfer thousands of gallons of water each day through the fountain, all of which can deliver an operating pressure of up to 16 bar.

With the pumps being able to operate at such a high level, the pumps are used in cycle rather than all at the same time making the system more energy efficient and cost effective.

Presidential approval
The Flame Fountain was officially opened in a ceremony held in the presence of the President, Illham Aliyev and his wife Mehriban. The city celebrated with a dynamic display of light, fire, water and music, creating different articulated water and light patterns making an unforgettable eye-catching show.

“The monument is in use all year round so a system of pumps which could maintain an efficient and consistent operation level was crucial.”
Using market leading products has created a pumping system which delivers energy and cost savings as well as reducing the need for regular maintenance.