It looks like you are coming from United States, but the current site you have selected to visit is Canada. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Thirsty work in Poland…

Sokpol

Poland

Poland-Lowara-Thirsty work in Poland….jpg

Lowara and Vogel have quenched the thirst for quality pumps within Sokpol, a leading Polish drinks manufacturer.

Application: Water supply

They constructed two deep-water wells and installed Vogel 88TV2SN/HM4D 1852F pumps controlled by a Hydrovar HV3.22, with a key requirement: an energy-saving solution with a frequency control converter that would, in the words of technical manager Piotr Kitala, “work on only as much energy as needed and which would eliminate pressure changes in the system.”

Lowara pumps are supplying the production lines with water. A three-pump system with vertical Lowara SVH 6005F150T pumps controlled by a Hydrovar HV3.15 (15 kW) have a capacity of 180m3 and provide aseptic, stable water pressure for cooling, washing, rinsing and filling the pasteurises. Another three-pump set with horizontal single-stage Lowara SHSH 50-200/110 pumps controlled by a Hydrovar HV3.11 (11 kW) supplies the water for the production of soft drinks and juices.

The aseptic environment enables Sokpol to get higher quality certification, and will help them remain the leading Polish company of soft drinks in cartons.

Editors note: We are continously modernizing our product portfolio: The Vogel deep well pumps are now the Lowara Z series, Lowara SVH the e-SV and SHSH the e-SH and Hydrovar the 5th generation Hydrovar.