It looks like you are coming from United States, but the current site you have selected to visit is Lithuania. Do you want to change site?

Yes, please! No, keep me on the current site

Flygt wins Innovative Technology Award

Flygt wins Innovative Technology Award

Xylem recently won a 2014 Innovative Technology Award from the Water Environment Federation (WEF) for the company’s wastewater pumping solution, Flygt Experior.

Flygt Experior’s clog-resistant design has been successfully field tested and proven to reduce energy consumption by up to 50 percent, with clog removal maintenance virtually eliminated. The award was presented to Xylem at the Water Environment Federation’s Annual Technical Exhibition and Conference (WEFTEC), the largest conference of its kind in North America.

Flygt Experior pumps incorporate state-of-the-art N-technology hydraulics, premium efficiency motors and intelligent controls in a package that is simple to install and easy to operate. These three complementary functions distinguish the fully integrated Flygt Experior system from traditional pump systems.

The muscle of the Flygt Experior is the premium efficiency motor coupled with ‘Adaptive N-hydraulics’ which further improves the results of the energy-saving, clog-free N-impeller. N-technology is suited for speed regulation as self-cleaning functionality is facilitated independently of rotational speed. Flygt SmartRun controls are pre-programmed with algorithms specifically designed for wastewater systems. The resulting pump performance delivers the ultimate in reliability, efficiency, and simplicity.

The self-cleaning Adaptive N-impeller was recognized by the WEF as the single greatest technology innovation during 2011. The Adaptive N-impeller moves axially upwards to allow easy passage of trash flow; the impeller then immediately returns to its normal operating position in close proximity to the volute insert ring eliminating clogging even under the most challenging conditions.

The Experior pumping solution now takes the wastewater industry one giant step further. “Extensive field trials in North America and Europe have proven that Flygt Experior not only eliminates major clogging problems but also deliver extended service intervals while significantly reducing energy costs,” said Lisa Riles, North America Marketing & Business Development Manager, Transport at Xylem Americas.

by Simon