It looks like you are coming from United States, but the current site you have selected to visit is Indonesia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Xylem’s Rule-Mate bilge pump: How to clean the sensor and return to level sense mode

If your Rule-Mate bilge pump is cycling on every 2.5 minutes but not running continuously, it has entered safe mode – a protective feature built into the pump's circuit board. This is normal behavior designed to prevent battery drain when the sensor area becomes fouled with debris, oil, diesel, or other contaminants. This video from Xylem's technical team explains how safe mode works, why it activates, and how to clean the pump's sensor to restore normal level sense operation.

How Rule-Mate safe mode works

Rule-Mate bilge pumps include an onboard circuit board with sensors that detect water at the impeller level. Under normal operation, called level sense mode, the pump activates only when water is detected.
 
If the sensor area becomes fouled, the pump may run continuously without actually pumping water. To prevent this, the pump's firmware is programmed to:

  1. Activate upon startup and monitor amp load.
  2. If no amp drop is detected (meaning the pump is not moving water), shut off automatically after approximately 15 seconds.
  3. Continue checking for water every 2.5 minutes by briefly spinning the impeller.
  4. Resume normal continuous operation as soon as water is sensed.

This 2.5-minute interval mode draws only 0.25 amps per day, so battery impact is minimal while the pump remains in safe mode.

How to return your Rule-Mate pump to level sense mode

Cleaning the sensor area is all that is required to exit safe mode. You will need a rag or toothbrush and mild soapy water.

Safety first: Disconnect power and remove the fuse before servicing the pump.

Steps

  1. Disconnect power: Remove the fuse before touching the pump.
  2. Remove the base: Detach the pump from its base to access the internal sensor board.
  3. Clean the sensor area: Use a rag, toothbrush, and soapy water to thoroughly clean the sensor area inside the base. Remove any debris, oil, or contaminants.
  4. Reassemble: Reattach the pump to its base and reconnect the hose.
  5. Restore power: Replace the fuse and reconnect power.

Once power is restored and the sensor area is clean, the pump will return to normal level sense mode and resume waiting for water before activating.

Frequently asked questions

Your pump has entered safe mode. This happens when the sensor area is fouled and the pump cannot confirm it is moving water. The 2.5-minute cycle is a protective feature. The pump checks for water briefly, then shuts off if none is detected.

No. In safe mode, the pump draws approximately 0.25 amps per day, which is minimal. Safe mode is specifically designed to protect your battery from the drain that would occur if the pump ran continuously without pumping water.

Common causes include bilge debris, oil, diesel fuel, or even a stray rag that contacts the sensor board inside the base of the pump.

A rag or toothbrush and mild soapy water are sufficient. No special tools are required.

Yes. Once the sensor area is clean and power is restored, the pump will automatically return to standard level sense mode.