It looks like you are coming from United States, but the current site you have selected to visit is Qatar. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode
< View all Making Connections
10 Principles of a Future-Proof Network

10 Principles of a Future-Proof Network

In order to drive customer satisfaction, utilities need to be smart.

In this day and age, the Internet of Things (IoT) has brought new meaning to the word “connected”. All over the world, machine to machine (M2M) communication has made possible improvements to citizen safety, efficiency, and sustainability on an unheard of scale. And many of those enhancements are increasingly being utilized by utilities to increase customer satisfaction.

In order to drive that customer satisfaction, utilities need to be smart. According to Randolph Wheatley, Sensus’ VP of Communications Solutions Marketing, “At its foundation, a smart utility has integrated capabilities that enable it to effectively gather information about the resources it provides and the network it uses.” But smart doesn’t just happen; it requires a communications network that can enable that potential. Here, then, are 10 principles to consider when implementing a future-proof utility network.

  1. Build for longevity
    Show network value as part of the solution years after deployment.
  2. Secure your data
    Maintain cybersecurity vigilance through encryption, layered defenses, and FCC-licensed spectrum.
  3. Perform preventative maintenance
    Extend the life of the network through regularly scheduled inspections and upgrades.
  4. Safeguard your infrastructure
    Build resilience by protecting network technology against extreme weather and natural hazards.
  5. Increase reliability
    Overlap coverage to provide backup in the event that a primary system fails.
  6. Reduce obsolescence
    Evolve with rapidly advancing technology that is critical in today’s fast-paced world.
  7. Plan ahead
    Anticipate and prepare for the future to ensure unforeseen problems are kept to a minimum.
  8. Review life cycle benefits
    Consider the tough to quantify, long-term benefits of the network during periodic reviews.
  9. Promote advantages
    Educate stakeholders on the benefits, advantages and capabilities that the network offers.
  10. Monitor and manage your bandwidth
    Prepare for ever-increasing volumes of data that drive expansion and new applications.

At its foundation, a smart utility has integrated capabilities that enable it to effectively gather information about the resources it provides and the network it uses.

Randolph Wheatley, Sensus’ VP of Communications Solutions Marketing

For more information, check out the Sensus video, “The Role of Smart Communications.” And if you’d like a deeper dive, we also offer a companion Viewpoint on the subject.

 

 

by Michael Tschirret
;