It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Function and use of dry run protection

The dry run protection accesory, protects your pump from running dry and getting damaged.

If the water level drops below the dry run protector, the controller will stop the pump and delay the restart for 15 minutes for the water level to recover. To force a quick restart, turn the controller off, then on again.

The dry run protection accesory must be positioned vertically, within 10°.

If the pump is not going to be installed vertically, find an alternative way to mount or suspend the dry run protection accessory, so that it is located higher than the pump and in a vertical position.

For more information, please click on the following link:

Using the pump in a horizontal position

Fixing and submersion depth

  • Along with the dry run protection accesory two cables ties are provided.
  • Clamp the accesory to the pipe just above the pump outlet as shown in the picture below.
  • The maximum submersion depth is 50 meters.

Connection to the controller

Connect the dry run protection accessory to the controller input as shown in the following video:

Activation

The dry run protection accesory can be activated in two ways:

  • Using the S-Connect application (with a Smartphone or tablet) and 
  • without using the S-Connect app, in case you do not have a Smartphone at hand.

To activate the dry run protection accesory via the app using a Smartphone, refer to the article below for more information:

Activate the dry run protection using the App

Managing sensor inputs and accessories with the S-Connect app

To activate the dry run protection accessory without using the S-Connect app, see the link below:

Activating the dry run protection without using the S-Connect app

Activation of accessories without the S-Connect application