It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Installing the pump in a well

Follow these steps to install the S1–200 in a well.

  1. Make sure the controller is turned off and all cables are connected
  2. Make sure the hose is connected tightly with the hose clamp
  3. Attach a safety rope to the pump (see video below)
  4. Slowly lower the pump into the well
  5. Attach the rope to a pole or similar robust structure next to the well

Further reading

Connecting a hose to your pump