Parece que vem de United States, mas o site atual que selecionou visitar é Portugal. Pretende alterar os sites?

Sim. Não. Mantenha-me no site atual.

Ative o modo de alto contraste

Dairy Plant Captures Biogas from Anaerobic Digestion

Containment liner, process piping and cover captures biogas from anaerobic digester to help diary meet sustainable growth goals

Laticínios Bela Vista Ltda. is the fifth largest dairy food producer in Brazil with three plants processing over 3 million liters of milk per day. The company makes over 100 different products for Laticínios Bela Vista's brands: Piracanjuba, Pirakids, Leitbom, and others.

Challenge

​Laticínios Bela Vista expanded their plant in Bela Vista de Goiás and evaluated wastewater treatment options that would meet the company’s commitment to sustainable growth and protection of the environment. Laticínios Bela Vista selected an anaerobic digestion treatment system proven to treat dairy wastewater. Anaerobic digestion also provides the added value of biogas that can be used as a fuel. The digester required a containment liner, process piping, and a gastight cover to capture the biogas.

Solution

Xylem was contracted to design and install the liner, piping, and cover for the 70 m x 140 m (230 ft x 460 ft) digester. The built-to-last geomembrane liner was especially designed for wastewater containment. Piping was fitted in the digester for influent, sludge, and effluent systems with supports and penetrations compatible with the geomembrane liner. The insulated floating cover​ was designed to collect the biogas generated by the digester, while providing safe access and low maintenance requirements for plants operators. The cover was custom-designed with hatches for mixers and ports for sampling. All components were made of materials sourced in Brazil.

Results

Xylem is proud to have provided a quality installation that helps Laticínios Bela Vista meet their goals for sustainable growth. The system is designed to generate 1,440 m³/h of biogas from the anaerobic digester, which is sent to the plant’s boiler, helping lower energy costs.

Laticínios Bela Vista​ will benefit from the value of the components provided by Xylem, including:

  • Containment of the wastewater and protection of groundwater resources
  • System control through internal pipework
  • Foul odor control
  • Thermal protection to enhance anaerobic digestion
  • Efficient and safe biogas collection for use as fuel
  • Low maintenance, including self-drainage of rainwater