It looks like you are coming from United States, but the current site you have selected to visit is Malaysia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Outsourcing Boiler Feed Water to Evoqua Proves Cost Effective

Solution provides more efficient operation and improved electrical service to Florida Power & Light customers

Challenge

Florida Power & Light (FPL) needed reliable water treatment equipment to produce boiler feed water at its Cape Canaveral plant, but faced the following challenges:

Less staff available to operate and maintain the plant's existing automatic regenerable deionizers
A need to reduce costs
The desire to eliminate chemical handling and disposal at the site

Solution

Evoqua Water Technologies and FPL entered into a long-term agreement under which Evoqua provides boiler feed water to the plant on a cost-per-1,000-gallon basis. FPL supplies the raw water, electricity and storage tank. Evoqua supplies the equipment and also operates and maintains the plant. This ensures a continuous supply of boiler feed water that meets FPL's specifications of 2 megohm-cm quality water with 10 parts per billion (ppb) or less of silica. Operation and maintenance costs are reduced, and there is no chemical handling or disposal required.

Evoqua built the metal building that houses the water treatment system, installed the equipment, started up the system, and has been operating it continuously since 1995. The 100-gallon-per-minute system includes: polymer injection; two 54-cubic foot multi-media filters; 54-cubic foot softener; bisulfite injection for chlorine removal; caustic injection for pH adjustment; twelve 30-inch 1-micron prefilters; reverse osmosis (RO) system; two FlexTrex® mixed-bed service deionizers.

Results

Before the agreement with Evoqua, FPL had five of their own technicians operating the water treatment plant. Now they rely on an Evoqua service technician who comes in once a week, or more often if needed, and changes the filters. FPL has partnered with Evoqua Water Technologies to design, build, own and operate water treatment plants at six other facilities: Fort Myers, Manatee, Port Everglades, Putnam, Riviera, and Sanford, as a way to operate more efficiently and improve electrical service to customers.