It looks like you are coming from United States, but the current site you have selected to visit is India. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Optimizing a plant's high purity water system with new CEDI modules

North America Utility uses Evoqua to modernize and optimize a competitors Continuous Electrodeionization System

Challenge

High-purity water is essential for producing steam that will not scale turbine blades with silica, minerals, and other contaminants. A large power generating company in North America used a competitor's continuous electrodeionization (CEDI) system for that purpose. Some of the challenges faced with the 2-year old system included:

  • The modules leaked profusely with water containing brine which caused scaling
  • The scaling led to electrical shorts and arcing which caused a fire in one of the trains
  • The replacement modules required up to six months for delivery
  • The replacement modules then failed continuously with one train of 28 modules lasting only ten months
  • Extensive manpower was required to maintain and replace the CEDI modules on a continual basis

Plant personnel had all but given up hope for the CEDI system. They needed technical expertise and a quick, dependable, leak-free solution.

Solution

Through the ReMod Program by Evoqua Water Technologies, which can be used to optimize existing CEDI and CDI systems and modules, Evoqua met with operating personnel from the utility and reviewed the current system, maintenance procedures, operating conditions, and expectations. 

After this meeting, Evoqua provided a plan to modernize the plant's high purity water systems.

Results

While still in progress, the existing CEDI modules within one train are being optimized with IONPURE® Technologies.

LX-MK modules. For the optimized train, benefits now include:

  • No leaks
  • No brine
  • No fires
  • Significantly reduced maintenance and replacement requirements
  • Less power consumption

Because of budgetary constraints, the existing power supplies are currently being salvaged and the second train is being rebuilt using the best of the existing competitor supplied modules.