Näyttää siltä, että lähtöpaikkasi on United States, mutta sivusto, jolla haluat nykyisen valintasi mukaan käydä, on Finland. Haluatko vaihtaa sivustoa?

Kyllä, kiitos! Ei, haluan pysyä nykyisessä sivustossa

Enable high contrast mode

Bush Brothers Wastewater Treatment Process Generates Green Energy

Anaerobic BVF reactor helps bean producer meet regulations while producing biogas to generate electricity

Bush Brothers is a family-owned corporation best known for its Bush’s Best® canned baked beans, which are made from a closely guarded secret recipe. This company produces the majority of the baked beans consumed in the United States.

Challenge

Bush Brothers’ manufacturing facility in Augusta, Wisconsin, USA, needed a new wastewater treatment plant, so it investigated different types of technology. The bean producer required a solution that would treat its wastewater so that it met environmental regulations. It also wanted to harness green energy from the treatment process.

Solution

ADI Systems was selected by Bush Brothers and its engineer, Donohue & Associates, to design an anaerobic digestion process. The low-rate anaerobic ADI-BVF® reactor was chosen to digest the bean processing facility’s wastewater.

  • ADI-BVF® reactor

    Anaerobic digestion system that offers very stable, robust wastewater treatment and biogas generation under a wide range of operating conditions.

ADI Systems’ design philosophy was to simply and efficiently treat the bean processing wastewater and, at the same time, produce biogas that could be used to generate electricity. The in-ground BVF® reactor easily meets these criteria with its large reactor volume for continuous and consistent organic removal, which provides stability to the downstream aerobic system.

The reactor became operational one month ahead of the scheduled commissioning date.

Results

The BVF reactor is digesting process wastewater and ground-up beans and consistently achieves over 90% chemical oxygen demand (COD) removal in the anaerobic effluent. The BVF reactor is self-regulating in pH, macro- and micronutrients; therefore, chemical addition is not required on a regular basis.

Biogas generated from the BVF​ reactor is treated and utilized in an internal combustion engine to produce electricity. Effluent from the facility is used for irrigation. Both Bush Brothers and ADI Systems are avid believers that the future of the business can be powered by green and sustainable energy at an affordable cost.

*All trademarks are those of their respective owner.