It looks like you are coming from United States, but the current site you have selected to visit is Australia. Do you want to change site?

Yes, please! No, keep me on the current site

Simplot Partners with Xylem on Wastewater Treatment Projects

ADI-BVF® reactor puts potato processor on fast-track to meet environmental regulations

The J.R. Simplot Company, commonly referred to as Simplot, is one of the largest privately held food and agribusiness companies. The company is headquartered in Boise, Idaho, USA, but it has operations around the globe, including Portage la Prairie, Manitoba, Canada, and Caldwell, Idaho, USA.

Simplot’s potato processing plant in Portage la Prairie processes frozen french fries and formed potato products. The potato products are sold to large, quick-service restaurant chains, as well as other customers.

Its facility in Caldwell processes traditional french fries (shoestrings, thin cuts, and regular cuts) as well as tater gems, hashbrown patties, and shredded hashbrowns.

Challenge

The two aforementioned Simplot potato processing plants were in need of new wastewater treatment systems. Simplot’s Caldwell plant needed upgrading in order to comply with environmental regulations. The company worked with various consultants and conducted studies to determine the best wastewater treatment solution. Later, when it came time for Simplot to build a new french fry plant in Portage la Prairie, wastewater treatment was again an important consideration, but it of course needed the appropriate technology.

Solution

Because of its positive experience working with Xylem in the past, Simplot once again selected Xylems’ wastewater treatment technology for two more projects:

Simplot’s Caldwell Plant

Xylem designed and built a 17 million gallon ADI-BVF® reactor for Simplot’s Caldwell plant. The anaerobic system treats effluent from the existing primary treatment plant and limits the suspended solids concentration to 350 mg/l. The reactor has the capacity to treat 2 mgd of primary wastewater with a chemical oxygen demand (COD) of 3,000 mg/l. This project was fast tracked so that it could be constructed before winter arrived.

Simplot’s Portage la Prairie Plant

Xylem designed and built a low-rate anaerobic BVF® reactor and aeration tank for Simplot’s Portage la Prairie plant. After fine screening to remove the skins and rejected potato material, the process wastewater is treated in a low-rate anaerobic reactor. The mud, or silt, is removed in a separate mud clarifier. The oily water stream is subjected to cooking oil removal prior to joining the mainstream process on its way to the anaerobic BVF reactor.

Biogas generated from anaerobic treatment at the Portage la Prairie plant is collected and burnt in its process boiler, helping to displace natural gas and cut operating expenses.

The anaerobic effluent is sweetened by oxidization of sulphides in an aeration tank equipped with subsurface aeration equipment. Sweetened effluent is then pumped through a 10 km (6 mile) force main to the city’s secondary plant for polishing prior to discharging effluent into the Assiniboine River. Some treated wastewater and stabilized anaerobic sludge is used to irrigate and fertilize agricultural land, helping nearby farmers.

Results

The BVF reactors that were installed by Xylem at both the Portage la Prairie plant and the Caldwell plant achieve approximately 86 percent COD removal rates. This allows Simplot to remain compliant with strict environmental regulations, and continue its commitment to natural resource protection. Because both reactors are covered with a gastight cover, the operations are essentially odor free.