It looks like you are coming from United States, but the current site you have selected to visit is Guyana. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Vortisand® Systems Reduce Medical Center's Cooling Tower Costs

Cross-flow media filtration reduces particles under 5 micron and improves maintenance and operational costs

The $500 million 434,000 square-foot, 6-story hospital building houses 262 beds and the adjacent medical office building is housed in a 172,000 square-foot, 6-story structure. In order to provide cooling and energy services to the campus, a 3-story, 31,800 square-foot central utility plant was included in the design.

The central utility plant includes three 3,000 GPM cooling towers and one 1,500 GPM cooling tower with the option to upgrade if needed. This hospital is located about 50 to 75 feet from a freeway with all 4 cooling towers facing the thoroughfare, exposing itself to the dusty air and debris. Being a hospital, it is run 24/7, with three 8 hour maintenance shifts.

With the need to filter contaminants from the water system, designers had originally specified centrifugal separators with bag filters as the side stream filtration technology. This technology works by separating particles from water using centrifugal energy and particle mass. The bag filters were used to filter small particles with the recovered water returned back to the system.

By the Numbers: 

$86,100 Maintenance Savings; $47,300 Energy Savings

Challenge

After a few months of operation a new challenge surfaced, maintenance costs were substantially increasing due to the cooling tower basins being cleaned on a weekly basis, along with the bag filters being replaced every shift due to the amount of dirt build up. Facilities Chief Engineer knew that this could not continue and embarked on a search for an efficient water treatment system.

J.D. Sales Co. presented Vortisand Cross-Flow Microsand Submicron Filtration as a possible water treatment system to resolve their dirt and debris related challenges. As particles smaller than 5 micron in size have been proven to be most likely to cause fouling and contamination in cooling tower systems, J.D. Sales Co. was confident that Vortisand was the correct technology for their side stream filtration project. Following this initial meeting, the customer was invited to visit a few existing installations that also used Vortisand systems for cooling tower side stream filtration. This included the new central utility plant at an international airport.

Solution

As part of the evaluation process a total operating cost calculation was performed. It was clear that significant maintenance savings would be achieved by replacing the centrifugal separators with a Vortisand® system. Thanks to its compact design, the Vortisand systems were able to be installed on the existing concrete pedestals that were used for the outgoing separators. An added benefit to the Vortisand system is that basin sweeper piping was not needed and eliminated during the retrofit.

Results

Upon start up, a laser particle analysis test was conducted, showing that particles of 5 micron and less in size made up over 95% of the particles within the cooling system water. After just 60 days of replacing the centrifugal separators with Vortisand a 90% removal of particles less than 5 microns was achieved.

"Over the last 6 months, I have to say that this was the best investment on a filter system that we could make. It has cut down on not just particulate, but it has also cut down on man hours on the maintenance. We no longer have to clean bag filters and our new system keeps the basins a lot cleaner than ever before."
Plant Operating Manager