It looks like you are coming from United States, but the current site you have selected to visit is South Africa. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Combined Sewage & Stormwater Handling

Solutions to address when CSO events challenge the capacity of a wastewater treatment plant or collection system

Combined sewers cause serious water pollution problems during combined sewer overflow (CSO) events. This occurs when combined sewage and surface runoff flows exceed the capacity of the wastewater treatment plant or the maximum flow rate of the system which transmits the combined sources. The overflow is often discharged to a receiving body of water that combines a variable mixture of untreated human and industrial waste, polluted runoff, debris and scoured materials that build up in the collection system during dry weather periods. Discharge contains a variety of contaminants such as chemicals, pathogenic microorganisms, viruses and cysts that impair water quality and impact human health and wildlife. Combined sewer overflows are the leading source of water pollution in the United States, with approximately 772 communities being susceptible as of 20171. 

Combined Pump Stations 

Combined pump stations are designed to handle the daily wastewater flows as well as stormwater and other surface run-off and are common in many wastewater networks. When designing a combined station, you should consider the normal fluctuations from the sewage network as well as the maximum inflow resulting from storm events. Both these inflow rates can differ widely from each other, and the maximum inflow can be much greater than the normal flow. 

Disinfection for Combined Sewer Overflow 

Factors to consider: 

  • Quality of the wastewater being discharged 
  • Potential toxic effects 
  • Ease of operation and maintenance 
  • Regulations governing residual standards 

Combined sewer overflow events occur intermittently and vary in flow rate, this makes it difficult to add and regulate a chemical disinfectant. Additionally, many CSO outlets are located in areas that are not readily accessible, leading to the requirement of an automatic system.