It looks like you are coming from United States, but the current site you have selected to visit is Romania. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Salt Water Disposal (SWD) Well Filtration

Screen Filters for Improved Water Quality and Reduced Maintenance in SWD Wells

A salt water disposal (SWD) well is a disposal site for water produced as a result of the oil and gas extraction process. Produced water, also referred to as salt water, contains particulate which can cause problems for the pump bringing water into the well. Prior to injection into an SWD well, it is highly beneficial for water filtration to be installed before the pump to prevent damage. 

Environmental agencies have regulations that vary by region to closely monitor the water disposal at SWD wells. While there are several factors to consider and varying levels of treatment necessary per well, some form of water treatment is required prior to injection into the well. Along with environmental concerns, improving the efficiency of the oil production process, as well as minimizing costs are becoming increasingly important.  

Xylem’s screen filters provide automatic cleaning and require limited maintenance, unlike bag filters that require frequent replacement and manual labor. Screen filters also do not have to be taken offline to backwash, whereas bag filters must be taken offline further slowing down production. Bag filter disposal creates additional challenges, including environmental and safety concerns, whereas Xylem’s screen filters pose minimal risk to the environment and service personnel. 

 

For every barrel of oil extracted, an average of 3 to 5 barrels of water are generated

Products & Services