It looks like you are coming from United States, but the current site you have selected to visit is Belize. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Upper Gwynedd Township, PA. Wastewater Treatment Facility

Managing peak wet weather flows cost-effectively within existing tankage

Challenge

The Upper Gwynedd Township, Pennsylvania wastewater treatment plant (WWTP) which treats residential waste (70 percent) and industrial waste (30 percent) was struggling to maintain performance during peak wet weather flows. The facility was designed to treat an average daily flow of 5.7 million gallons per day (MGD) and a maximum monthly flow of 6.5 MGD with a peak hourly flow of 12 MGD. Water quality would deteriorate when the plant attempted to treat these peak flows, as the clarifier became the bottleneck due to lack of solids separation.

With the facility struggling to treat its original peak design flow of 12 MGD, the plant used its available tanks to hold and equalize the flow as much as possible. The monitoring and controlling of these high-flow events was a time-consuming, operator-intensive process. 

In addition, a potential future total phosphorus (TP) limit of 0.2 mg/L was another requirement to consider an upgrade to their system. 

Solution

To avoid the expense of tertiary treatment and a secondary treatment system upgrade, Upper Gwynedd installed the BioMag® system with the assistance of the engineering firm, Environmental Engineering & Management Associates.

Evoqua's magnetite ballasted clarification process met the plant's needs without additional tankage, in-basin changes, or flow diversion during construction avoiding any treatment interruptions. The BioMag® system’s fast settling rates allow it to operate with elevated concentrations of mixed liquor suspended solids (MLSS). The system also improved the quality and stability of the Township’s effluent to the extent that the plant will be rerating to an annual average flow of 6.4 MGD, a maximum monthly flow of 7.5 MGD and a peak hourly flow of 22.5 MGD.

Unlike other high-rate clarification technologies, the BioMag® system is compatible with any type of clarifier.

Results

Initial Pilot Testing

During initial pilot test of the BioMag® system, it was able to adequately treat all flow (hydraulically and organically), as well as reduce TP below the future limit of 0.2 mg/L. The pilot achieved: 

  • Stable, high-level treatment at elevated flows of 6+ MGD using
    half of the available clarifiers, which corresponds to a peak
    hourly flow of 12+ MGD 
  • Stable, high-level treatment at organic loading comparable to 10,842 lbs. per day, which is the maximum biological oxygen demand it was designed to manag
  • A lower effluent TP limit of 0.2 mg/L without adding new tankage or additional tertiary treatment steps, while maintaining consistent control over the sludge
    blanket throughout a wide variety of process conditions
  • Total suspended solids (TSS) of less than 10 mg/L (monthly average) and less than 30 mg/L (maximum per day) during
    peak flows
  • Consistent nitrification and met ammonia permit levels (summer 0.74 mg/L, winter 2.2 mg/L) during design loading conditions

In the summer of 2007, a pilot of the CoMag​® system proved its ability to meet the new TP limit with alum, polyaluminum chloride (PACL), ferric chloride or sodium aluminate coagulants.  Additionally, the pilot proved that the CoMag® system could meet future permit limits as low as 0.05 g/L without polishing filters by simply increasing the coagulant dose.  

Full-Scale Installation Results

Since it was first installed in early 2014, the BioMag® system has been successfully handling high wet weather flows and producing effluent with TSS concentrations below 10mg/L and carbonaceous biological oxygen demand (CBOD) of less than 5 mg/L during these conditions.

Additionally, Upper Gwynedd Township completed two, seven-day performance tests in September 2014 and March 2015. The facility had to meet a 0.2 mg/L effluent phosphorous limit each time. It successfully passed with an average effluent reactive phosphorous concentration of 0.09 mg/L and 0.11 mg/L in September and March, respectively.

The Ultimate Stormwater Test

In April 2014, the BioMag® system successfully passed the ultimate stormwater test — a once-in-a-lifetime, five-inch rain event. The effluent TSS increased to 8 mg/L during the storm. Almost all of the other WWTPs in the Philadelphia area were flooded, but Upper Gwynedd’s BioMag® system easily handled the excess flow.