It looks like you are coming from United States, but the current site you have selected to visit is South Korea. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Bioxide® solution reduces odors, corrosion, and complaints

Challenge

Xylem was contacted by a Mid-Atlantic Water Authority to propose an odor control solution at one of their pump stations. The Authority was treating the odors with a sodium hypochlorite (bleach) solution to varying degrees of success. Downstream hydrogen sulfide levels in the atmosphere were the primary contributors to odor complaints, reports of corrosion, and worker safety issues. Xylem had provided other odor control solutions at a different location for the Authority previously, but this site was still using a legacy solution.

The customer also had chlorine nuisance odors at the bleach dose site. This caused pump station component corrosion, worker complaints and irritation, so a non-hazardous solution was preferred. Background data collected with bleach dosing at a rate of 1,200 gpd showed a treated level of dissolved sulfide of 1.5 mg/l and an average of above 40 ppm of atmospheric hydrogen sulfide at the control point.​

Solution

Xylem evaluated the situation and determined that BIOXIDE®​ Calcium Nitrate Solution was the best treatment method. Bioxide solution contains no hazardous substances and is a safe, easy-to-handle method of odor control. It also reduces future corrosion by effectively eliminating dissolved hydrogen sulfide.

The Mid-Atlantic water authority was a little apprehensive about using a non-chemical product. As a result, Xylem offered to provide on-site testing to evaluate performance.​

Xylem provided complete, turnkey services with safety trained personnel, working with the customer to empty the existing bleach tanks, safely clean them out, and install a new dosing controller. The Mid-Atlantic water authority utilized our full service odor control program, consisting of BIOXIDE Solution​​​, VersaDose® LT dosing controller, and VaporLink® online atmospheric hydrogen sulfide monitors. The system provides remote monitoring and dosing control with 24 hour, 7 day set points to optimally treat varying hydrogen sulfide levels.

Results

Xylem worked closely with the customer to determine dosing rates and profiles for optimal odor control. Final summertime feed rates were roughly 400 gpd, with a < 2 ppm average atmospheric hydrogen sulfide at the control point.

After reviewing the final results and feed rates, the customer elected to continue with Bioxide solution. Xylem quickly provided the customer with a working system and met their goals of reducing hydrogen sulfide odors and nuisance chlorine gas issues​.​