It looks like you are coming from United States, but the current site you have selected to visit is Greece. Do you want to change site?

Yes, please! No, keep me on the current site

How to Check the Barrier® M UV Sensor

Follow the steps below to check the UV sensor

The displayed value of the unit sensors has to be checked with a comparative measurement with a reference radiometer. The value measured with the unit's UV sensor may not exceed more than 5% above the valued measured with the reference radiometer. This value should also not be significantly below the value reduced by the measuring uncertainty. If this is case, the cause has to be determined and eliminated (soiling). If necessary, the UV sensor has to be replaced with another sensor with a valid calibration certificate; the new sensor then has to be checked and recalibrated by an approved organization.

The comparative measurement with a reference radiometer takes place when the unit is in operation. The lamps must be on for at least 15 minutes without interruption.

Keep in mind the following instructions are meant to be a general guideline. Always refer to the owner's manual for your specific UV system.

1. Enable the "Test mode" function in the operator menu

For the duration of the check/control measurement (set at factory to 120 s), the alarm or switching functions are disabled.

2. Unscrew the union nut from the measuring glass

3. Pull the UV sensor out

4. Insert reference sensor and check displayed value

5. Put the unit's UV sensor back in

6. Screw the union nut into place

7. Alarm or switching functions are Now enabled

After the test time of 120 S has expired.

Safety Tip

The proper function of the monitoring unit has to be checked at regular intervals. Make sure to check it at least semi-annual.