It looks like you are coming from United States, but the current site you have selected to visit is Yemen. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Different Types of Pure Water for the Lab: What You Need to Know

Making the decision on which type of water you need for your application can be challenging. Xylem can help.

There a several types of water purity available depending on what you’re tackling at the bench, from Type III for general use such as rinsing out your beakers, all the way up to Type I+ for sensitive applications like graphite furnace atomic absorption spectrometry (GF-AAS). Making the decision on which type of water you need for your application can be challenging.


How is Laboratory Water Purity Assessed and Defined?

To implement a coherent classification system for water purity, we make use of several key factors describing the various properties of water.

The Conductivity of Water

Conductivity is reported as microSiemens per centimeter (µS/cm) at 25oC and is the reciprocal of resistivity and provides a measure of a fluid's ability to conduct electrical current. Conductivity is typically used when assessing water ranging from 'raw water' to 'drinking water' and provides a valuable, non-specific indication of the level of ions in the water.

The Resistivity of Water

Reported as Megohms per centimeter (MΩ-cm) at 25oC, resistivity is related to conductivity: a high resistivity equals a low conductivity. As such, it also provides a measure of the water's ionic content. Unlike conductivity, resistivity is primarily used in the assessment of ultrapure water.

Organic Compound Levels in Water

Organic compounds can exist in water in numerous forms, thus measuring every single one individually is impractical. The most useful indicator is the total organic carbon (TOC) content of the solution. This is measured via a process that oxidizes the organic compounds present and then quantifies the oxidation products generated. TOC is as close as we can get to a 'universal indicator' for the presence of organic impurities.

Alternatively, chromatographic techniques may be employed to determine the specifics of organic content, but this is frequently considered both too expensive and time-consuming to be used in general monitoring workflows.

Biological Contamination of Water

The presence of biological contaminants such as bacteria and other microorganisms is a common issue in untreated water. Bacterial levels reported as colony forming units per milliliter (CFU/ml) are kept low via filtration, UV treatment and sterilant solutions. Following an incubation period in suitable growth media, individual bacterial species and total viable cell counts can be determined. Bacteria counts may also be monitored through the use of epifluorescence testing to rapidly detect and distinguish between dead and living microorganisms.

In addition to the bacteria themselves, endotoxins produced from the cell wall of gram-negative microorganisms (reported as endotoxin units per milliliter, EU/ml; 1 EU/ml approximately equal to 0.1 ng/ml) can be assessed using standard tests based on Limulus Amebocyte Lysate activity.

The Presence of Colloids in Lab Water

Suspended particles can cause water turbidity (measured in Nephelometric Turbidity Units, NTU) and are therefore filtered out of laboratory water as much as possible. This colloidal material is defined as being less than 0.5 µm in size and may contain iron, silica, aluminium or organic materials. The Fouling Index (FI) is frequently used to estimate the potential of water to block filters under 0.45 µm filter conditions.

Setting the Standards of Water Purity

There are several international boards around the world that have been working to establish some degree of consistency in the standards of water purity – the more people we have agreeing to these standards, the easier it is to generate reproducible data. Some labs will also adopt standards as outlined by the regulatory body overseeing the region they work in, for example, as found in the European, US or Japanese Pharmacopoeias. However, very few of these standards are specific to a particular application.

Clinical and Laboratory Standards Institute (CLSI) – formerly NCCLS

As of 2006, the CLSI has moved away from the typical Type I, II and III designations, instead preferring to suggest that water be simply ‘fit for purpose’, and only describes one grade in significant detail: Clinical Reagent Laboratory Water. The CLSI has also briefly outlined other grades in less detail, such Special Reagent Water (SRW) and instrument feed water.

International Organization for Standardization (ISO)
The ISO based its specification on ISO 3696:1987, and specifies three grades of water: Grade 1, Grade 2 and Grade 3, where Grade 1 is the most pure (see below):

Water quality parameters for ISO grades

Parameter Grade 1 Grade 2 Grade 3
pH value at 25oC  --  -- 5.0-7.0
Conductivity (μS/cm)  at 25oC, max 0.1 1.0 5.0
Oxidisable matter Oxygen content (mg/l), max -- 0.008 0.4
Absorbance at 254 nm and 1 cm optical path length, absorbance units, max 0.001 0.01 --
Residue after evaporation on heating at 110oC (mg/kg), max -- 1 2
Silica (SiO2) content (mg/l), max 0.01 0.02 --


American Society for Testing and Materials (ASTM)

The ASTM uses D1193-06 and has four grades of water (see table below):

Water quality parameters for ASTM types

Parameter Type I* Type II** Type III*** Type IV
Conductivity (μS/cm) at 25oC, max 0.056 1.0 0.25 5.0
Resistivity (MΩ-cm) at 25oC, max 18.0 1.0 4.0 0.2
pH at 25oC -- -- -- 5.0–8.0
TOC (μg/l), max 50 50 200 No limit
Sodium (μg/l), max 1 5 10 50
Sodium (μg/l), max 3 3 500 No limit
Chloride (μg/l), max 1 5 10 50


*Requires use of 0.2 μm membrane filter; **Prepared by distillation; ***Requires the use of 0.45 μm membrane filter

Selecting the Right Water Purity Type

It may be overwhelming to know what type of water system you need. We have local sales reps who can help you select the right purification system for your application. Contact us to learn more.