It looks like you are coming from United States, but the current site you have selected to visit is France. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode
< View all Making Connections
Strain on the Grid: Why It’s Time to Rethink Legacy Powerline Carrier Systems

Strain on the Grid: Why It’s Time to Rethink Legacy Powerline Carrier Systems

The rapid growth of electric vehicles (EVs) and the expansion of data centers are transforming the energy landscape. Technological advances place significant stress on the aging electrical grid, causing utilities to grapple with fluctuating energy demand to keep the lights on. Unfortunately, many utilities are reliant on powerline carrier (PLC) systems, a legacy solution that struggles to keep pace with the evolving grid

Upgrading to Advanced Metering Infrastructure (AMI) offers the reliability, scalability, and efficiency needed to build a secure energy future. 

The Challenge at Hand

Electric utilities face a growing list of challenges. From aging infrastructure to escalating risk management demands, these organizations are under immense pressure. EVs, with their high-charging loads, require utilities to deliver significant power over increasingly dynamic schedules. Large-scale AI and data centers operate around the clock, consuming vast amounts of electricity to sustain servers, cooling systems, and storage. These pressures overwhelm outdated PLC systems, which lack bandwidth, real-time visibility, and flexibility to adapt.

By relying on existing electrical wires for communication, PLC systems face inherent limitations, including slow data transmission rates, inadequate outage information, and restricted visibility over customer usage patterns. These obstacles not only hinder proactive grid management but can also compromise efficient energy distribution and overall reliability. 

Why PLC Systems Are Falling Short

At its core, a PLC system is a one-way street. It transmits limited data from customer meters back to the utility, often too intermittently to provide actionable insights. PLC systems struggle to meet the intricate demands of modern utilities.

Key Limitations of PLC Systems:

  • Outage Management: During widespread outages, PLC systems only report failures through delayed, periodic polling, slowing response time.
  • Connectivity Issues: Transmission is often disrupted across geographically diverse or heavily populated areas, leading to gaps in data and operational delays.
  • Limited Bandwidth: With energy loads expanding, the system’s capacity to transmit accurate, granular information falls short.

These limitations make upgrading to a more advanced, flexible system not just beneficial but essential for ensuring reliable energy delivery.

Enter Advanced Metering Infrastructure (AMI)

The shift from PLC to AMI represents a paradigm shift in utility management. Unlike their predecessors, AMI systems offer two-way communication, enabling real-time data collection and faster response rates.

One standout feature of AMI systems is the adoption of point-to-multipoint (PTMP) architecture. By using licensed radio frequencies to communicate directly with endpoints, PTMP systems deliver unparalleled performance and reliability.

Benefits of AMI with PTMP Architecture

Scalability to Meet Demand

With the surge in energy consumption, utilities need infrastructure capable of scaling alongside growing demand. PTMP architecture provides an extended range and high-capacity data transfer, empowering utilities to manage real-time power flow even in high-demand scenarios.

Real-Time Visibility

Unlike PLC, which relies on intermittent polling, AMI systems offer instant updates. Real-time energy consumption data from EV chargers or sensor modules in data centers can be accessed at a granular level, helping avoid grid congestion and ensuring energy efficiency. 

Enhanced Outage Management

During large-scale outages, PTMP networks shine. Each endpoint sends outage "last gasp" messages directly to the utility, providing precise locations of failures. This capability can reduce restoration times by as much as 33%, as utilities deploy crews exactly where they are needed.

Bi-directional Flow Support

EVs, solar panels, and battery storage are driving the rise of two-way energy flows. PTMP AMI systems are well-equipped to handle reverse energy data, enabling utilities to credit energy suppliers and balance grid load.

Building Resilience for the Future

The increasing complexities of energy demands are pushing outdated PLC systems beyond their limits. Transitioning to advanced metering infrastructure with point-to-multipoint architecture provides utilities with the resilience, reliability, and adaptability needed for a modern, dynamic grid. This is more than an upgrade; it is a step toward building smarter, more sustainable energy networks that can deliver reliable service and adapt to the future. Making the switch now will prepare utilities for resilient operations, ensuring they meet and exceed the needs of the communities they serve.

;