Het lijkt erop dat u van United States komt, maar de huidige website die u wilt bezoeken is Netherlands. Wilt u van website wisselen?

Ja, graag. Nee. Ik wil op de huidige website blijven.

Lowara Circulators. The Go-To Solution for Plumbers and Installers

In the commercial and residential building space, plumbers and installers encounter various challenges on a daily bases, such as limited installation spaces or malfunctioning  pumps, often leading to heat loss, noise excess, flow rate issues, corrosion or even worse clogging, resulting into an increased number of times technicians have to return to a job site to fix issues that were not resolved during the initial visit. 

“We collaborate closely with plumbers and installers on a global scale and their primary need is clear: pumps that are easy to install, function reliably, and minimize callbacks “, says András Kovács, Senior product manager, Circulators. “Lowara ecocirc circulators are designed to address these needs, focusing on the requirements of those who select, install and service them”.

Here is why Lowara Circulators Are the Top Pick for Plumbing Professionals

  • Fast & Easy Installation. Installers appreciate the simplicity of the setup process. Features such as a single control knob, compact size, and automatic air-purge facilitate quick installations, even in challenging retrofit scenarios.
  • Built for Real-Life Conditions. The patented Anti-Block Technology helps prevent issues caused by sludge and magnetite, particularly in older systems. Additionally, dry-run protection and robust design enhance reliability and peace of mind.
  • Reduced energy Consumption. Lowara ecocirc circulators can reduce energy consumption by up to 80% compared to older fixed-speed models, aiding installers in meeting efficiency regulations and reducing long-term costs for end users. As an example , in a typical 120 m² German household with four residents, two circulators are often used, one for heating and one for domestic hot water recirculation. Replacing both with modern Lowara ecocirc pumps can reduce electricity usage by approximately 600 kWh per year, saving around €210 annually on energy bills. This also translates to a yearly reduction of approximately 200 kg of CO₂, equivalent to driving over 1200 km in a petrol car, demonstrating significant environmental and financial benefits.

Energy savings are indicative and based on comparisons with traditional fixed-speed circulators operating under similar conditions. Actual savings may vary depending on system design, usage patterns, and local electricity prices.

  • Made in Europe. Every Lowara pump is designed and manufactured in Europe, adhering to the highest industry standards and supported by rigorous third-party certifications, including CB report and A2L compatibility. This ensures dependable quality, contrasting with the uncertainties associated with some low-cost imports.
  • Best Value for Money. Lowara ecocirc pumps provide high performance at an affordable price, a combination that encourages professionals to choose them repeatedly for different projects. While some circulator manufacturers emphasize high-end features that are seldom utilized on-site, Lowara ecocirc prioritizes essential functionalities, ensuring practical benefits in real-world installations.

The Lowara ecocirc series delivers what professionals value the most: easy installation, reliable performance and lower energy bills, all supported by a trusted global brand.

 

 

 

 

 

 

 

 

About Xylem

Xylem (XYL) is a Fortune 500 global water solutions company that empowers customers and communities to build a more water-secure world. Our 23,000 diverse employees delivered combined pro forma revenue of $8.1 billion in 2023, optimizing water and resource management with innovation and expertise. Join us at www.xylem.com and Let’s Solve Water.