It looks like you are coming from United States, but the current site you have selected to visit is Bahrain. Do you want to change sites?

Yes, please. No. Keep me on the current site.

How Does the Pump on a Jabsco Manual Toilet Work?

Curious about how a Jabsco manual marine toilet works? Here our team demonstrates how the pump works in our Jabsco Twist 'n' Lock marine toilet. We manufacture the inside components of our manual marine toilets to be super simple, making it easy for assembly and for servicing the pump.

[Video Transcription]

Jeff: Thanks for watching jabscotech.com. I'm Jeff Lander.

Mike: And I'm Mike Irving.

Jeff: And today we're going to show you just exactly how a manual toilet works.

Mike: Bob, our machinist, he did a cool cutaway on our manual pump assembly. I'm going to get behind the camera and Jeff’s going to walk you through it.

Jeff: So now I'm going to talk about the wet bowl operation of the pump. During wet bowl operation, the top valve gasket and the brass fitting are sitting flat, which allows the necessary vacuum to prime. Now, since the manual pump is a dual action pump, I like to use a little expression to describe its operation. When the waste goes in, the water goes out, and when the waste goes out, the water goes in. So what exactly does that mean? When I lift up on the handle, waist is being brought in from the bowl into the lower half of the pump assembly below the O-ring. During this process, water is being brought out of the pump assembly into your bowl. So, again waste in water out. Now when I push down on the handle, this is waste out, water in. So when I push down, waste is being evacuated from the pump assembly down your discharge hose line. And the water in is coming from the valve cover into this upper half of the pump chamber.

So now I'm going to talk about the dry bowl setting. When you flip to the dry bowl setting, what happens is the little cam finger housed inside of the pump assembly lifts up on this little brass coiner fitting. So I'm going to do it a couple of times to show you the exact motion. Notice when I flip it over to the dry bowl, that little selector level pushes up just a little bit on that coin. On the flip side, you can see how the cam swings in and out when I switch back and forth between the dry bowl and the wet bowl settings. So just like I told you before, that little expression, all we're doing is replacing water with the word air. So when they lift up on the pump handle, this fills the pump chamber with waste and expels air into the bowl. When I push down, this pushes the waste out of the cylinder, into your discharge hose line and brings in air into the cylinder. So again, lift up, bring waste into the cylinder, bring air into the bowl. Push down, expel the waste, bring air into the chamber.

So there you have it. We just showed you a quick little video showing how exactly the manual toilet works.

Mike: That was pretty cool. With the cutaway that we made we're able to show you what happens when you bring the handle up and push it down. My name is Mike Irving.

Jeff: I'm Jeff Lander. This concludes this episode of jabscotech. Check back soon. We'll have more videos for you.