It looks like you are coming from United States, but the current site you have selected to visit is Indonesia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Jabsco Macerator Blown Fuse Diagnosis

Is your Jabsco 18590 macerator popping fuses? This video will show you a quick way to diagnose the macerator and determine if you need a service kit or a new pump.

[Video Transcription]

Jeff: Thanks for watching jabscotech.com. I'm Jeff Lander.

Mike: And I’m Mike Irving.

Jeff: And today, we're going to talk about the 18590 series macerator popping the breaker.

Mike: We're going to show you one quick way to figure out if it's going to be a motor issue or if it's just going to need a service kit.

Jeff: Thanks, Mike. Let's get at it.

Mike: Normally your macerator looks just like this. But what we did is we did a cutaway; it’ll give you a bird's eye view of what's going on inside of that pump.

All right. First things first. Wear rubber gloves and also disconnect the power. On the very end of the motor you're going to find this little bumper. Pop that bumper off and with a flat screwdriver, give that shaft a couple turns counterclockwise. If you notice up here, what we're doing is we're rotating the shaft, which spins the impeller. If this unit's been sitting for a little while, what it's going to do is it's going to free up that motor and free up that impeller in there. Now go ahead and reattach the rubber bumper and apply power. If the unit runs, you're good to go. If it runs for a few seconds, you might just need a service kit to replace the upper components here. If it doesn't run at all, you might consider purchasing a new 18590 macerator.

We just showed you one quick tip to try to get you back up and going again.

Jeff: If it didn't work, you have a couple of options. You can try a service kit which is a part number of 18598-1000 that will give you all the necessary components to do a complete rebuild. You know if you don't want to get down and dirty you can replace the entire unit. You know the 12-volt version has a part number 18590-2092. If you have a 24-volt version, it's a 18590-2094. Or if your macerator label reads 18590-2592, it's actually the same as the retail 18590-2092, and the same applies for your 24-volt version. Thanks for watching jabscotech.com. I'm Jeff Lander.

Mike: And I’m Mike Irving.

Jeff: Stay tuned for more jabscotech videos coming soon.