It looks like you are coming from United States, but the current site you have selected to visit is Greece. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Future-proofing data centres starts when minimum compliance stops

By Igor Chodaton, International Business Development Manager Large Projects - Data Centres, Xylem

The data centre industry is in a demanding phase. Growth is accelerating and the conversation is changing. Operators, consultants and specifiers are being asked tougher questions about power, water, carbon and community impact.

Sustainability starts at design stage

Sustainability is often treated as an outcome when, in reality, it’s shaped much earlier. Whether or not a facility can meet expectations around power usage effectiveness (PUE), water usage effectiveness (WUE) and carbon usage effectiveness (CUE) is determined long before it becomes operational.

Today, expectations go further. Metrics such as Energy Reuse Effectiveness (ERE) reflect growing pressure for data centres not only to minimise impact, but to contribute value back to local energy systems. The ability to recover and reuse waste heat, for example, depends on foundational design choices - from cooling architectures to how facilities connect with surrounding infrastructure.

Those metrics are influenced by early choices around cooling, pumping, water management and control. That’s why sustainability in data centres can’t be treated as a reporting exercise or an afterthought. It has to be designed in.

Inefficiency builds costs into the system

Poor decisions at the design stage can lock in higher energy use, greater water dependence, increased operating cost and avoidable lifecycle emissions for years to come. Once inefficiency is designed into a facility, it will be repeated every day. Every unnecessary kilowatt adds to the carbon burden over the lifetime of the centre.

Carbon reduction matters not simply because the industry is under greater scrutiny, but because higher energy demand means higher emissions, year after year. In a sector where facilities are expected to perform for decades, that’s a long-term design liability rather than a short-term operational issue.

Future-proofing means engineering beyond compliance

Future-proofing is won or lost at the design stage. Data centres should be judged not only by the resources they consume, but also by how intelligently they’ve been planned to reduce them.

In an environment shaped by performance demands, sustainability expectations and pressure to justify new developments, minimum compliance is a fragile benchmark for the future. The facilities best prepared for what comes next will be those engineered beyond today’s baseline.

Higher-efficiency systems are moving the industry forward

In the fast-changing data centre landscape, systems need to do more than comply. Technology is creating practical opportunities to reduce energy demand and help operators respond to rising expectations with greater confidence.

Modular, scalable system design, supported by advances in IE5 motor efficiency, intelligent variable-speed control, digital monitoring and adaptive water-system design, is helping operators build centres that are more efficient, more robust and more responsible in the way they use energy and water.

Xylem brings the full system into view

At Xylem, we know the next generation of data centres will be defined by the intelligence of the systems designed into them. They’ll also be judged by how well they’re prepared for rising expectations around performance, sustainability and public acceptance.

That thinking runs across Xylem’s portfolio, bringing together high-efficiency pumping, intelligent control, digital monitoring, water treatment and water stewardship from the outset. Within the Lowara range in particular, IE5 motor efficiency and smarter system design are helping create practical opportunities to reduce energy consumption by up to 40% within pumping and water systems, depending on baseline and design.

Designing for what comes next

The next phase of data centre growth will be shaped by engineering decisions that go beyond minimum compliance, reduce energy demand and build in long-term efficiency from day one.

The facilities best prepared for the future will be those designed to respond to rising technical, regulatory and public expectations. That’s what will separate data centres built to satisfy what’s required today from those created for what’s coming next.

Future-proofing data centres is won or lost at the design stage—long before operations begin.