It looks like you are coming from United States, but the current site you have selected to visit is Azerbaijani. Do you want to change site?

Yes, please! No, keep me on the current site

EnviroMix takes biological phosphorus removal to the next level with BioMix and BioMix-DC

Wastewater Treatment Facility in Stonegate Village, CO  

Wastewater Treatment Facility in Stonegate Village, CO  - anoxic and anaerobic selectors
BioMix is used to continuously mix the anoxic selectors that follow the anaerobic selectors. 

Stonegate Village Metropolitan District (SVMD) serves a population of approximately 11,000 near Parker, CO, and is responsible for providing a variety of vital services, including wastewater treatment.

Challenge

In 2014, SVMD hired Burns & McDonnell to evaluate options for upgrading the wastewater treatment facility. The existing equipment had reached the end of its design life, and the facility could not meet future water quality discharge standards. A comprehensive upgrade and expansion were needed to improve performance, including an advanced process for biological nutrient removal and hollow fiber membrane separation designed to meet a permitted effluent total phosphorus concentration of less than 0.05 mg/l.

Solution

EnviroMix’s BioMix Compressed Gas Mixing technology was well-suited for SVMD’s upgrade. The existing treatment tanks were converted to selectors and digesters and configured as eleven small zones — which would have required more than 24 mechanical mixers. By contrast, BioMix leverages a low-maintenance centralized compressor system, providing optimal mixed process conditions for the anaerobic, anoxic, and deox selectors, as well as the anoxic digesters. Compared to mechanical mixing technology, BioMix reduced annual maintenance by an estimated $20,000 and decreased O&M costs by 90%.

Phase II

After seven years of operation with BioMix, SGVM was excited to upgrade their anaerobic selectors to a BioMix-DC Enhanced Anaerobic Mixing System. Released in 2021, BioMix-DC was the 2022 winner of the Water Environment Federation (WEF) Innovative Technology Award. Due to very stringent effluent phosphorus requirements during the winter months, SGVM initiated BioMix-DC operation in August 2022 as an early adopter of the new technology.  

Wastewater Treatment Facility in Stonegate Village, CO - BioMix-DC nozzles
BioMix-DC nozzles provide gentle pulses of mixing energy to transport VFA from the fermentation layer to the PAOs throughout the anaerobic selector. 

BioMix-DC optimizes bio-P by transforming a traditional anaerobic selector into an intensified fermentation tank by alternating a short mixing cycle with a long deep cycle. The deep cycle stratifies the reactor to increase anaerobic solids retention time (SRT) and create a fermentation blanket to generate volatile fatty acids (VFA). The presence of additional VFA leads to the proliferation of PAOs, the microorganisms responsible for bio-P. Testing in SGVM’s anaerobic selectors demonstrates that the concentration of sCOD in the fermentation layer is more than 10X higher than in the bulk liquid (the volume of the reactor above the fermentation layer), indicating an abundance of VFA.  

Results

The BioMix upgrade in 2014 resulted in 50-60% energy savings compared to mechanical mixing and reduced annual maintenance cost by as much as $20,000. By upgrading to BioMix-DC operation in 2022, SGVM is expecting to reduce chemical consumption due to increased stability of the biological phosphorus removal process. 

Wastewater Treatment Facility in Stonegate Village, CO - BioMix-DC results chart
Powerful BioMix-DC results. 

0,25HP/1,000 Cubic FT Mixing Efficiency

1,10 MGD Design Flow (ADF)

“We have used EnviroMix products since 2015. The mixers work efficiently with minimal maintenance requirements.”
Kyle Chisholm, Lead Operator