It looks like you are coming from United States, but the current site you have selected to visit is Azerbaijani. Do you want to change site?

Yes, please! No, keep me on the current site

Less noise, more comfort: the smart evolution of hydronic installations

Marco Dola, Product Manager, Booster Sets and HVAC Pumps, AW, Xylem

In hotels, residential buildings, and modern office facilities, the level of comfort perceived by guests, residents, and employees depends on many factors: air quality, temperature, and natural lighting. Yet there is one element that is often underestimated during the design phase and can significantly affect the overall building experience: noise generated by hydronic systems.

Pressure boosting systems, HVAC circuits, and lifting systems are now essential components of any modern building. When they do not operate under optimal conditions, they can become a significant source of vibrations and noise within living and working environments, so much so that Italian regulations on passive acoustic requirements for buildings specifically address noise generated by plumbing and HVAC systems.

Why noise and vibrations occur in hydronic systems

Noise and vibrations rarely stem from a single cause. In most cases, they are the result of operating conditions that place stress on the system and compromise its smooth operation. One of the most common situations involves systems designed to handle peak demand conditions that occur only during limited periods of the day. Under these circumstances, pumps operate far from their best efficiency point, creating conditions that encourage turbulence, cavitation, and premature wear of components.

Another critical factor is the constant start-stop cycle typical of fixed-speed systems. Sudden pressure variations can cause the so-called water hammer effect, perceived as shocks, vibrations, and noise throughout the distribution network. Over time, these stresses can also affect the overall reliability of the installation. In addition, vibrations tend to propagate through piping systems and fixing points into occupied spaces, negatively impacting perceived comfort even far from the pumping room.

In residential buildings, hotels, and office facilities, where water booster systems are often located close to rooms, apartments, or shared areas, even a few decibels can make the difference between comfort and discomfort. Acoustic comfort guidelines for office spaces indicate recommended noise thresholds between 35 and 55 dB depending on the intended use of the space — levels that poorly managed systems can easily exceed.

Why intelligent control makes the difference

Reducing noise and vibrations does not depend solely on the mechanical design of the system, but also on how the installation is managed. Intelligent speed control allows pumps to continuously adapt to the actual demand of the building, enabling:

  • smoother operation with fewer pressure fluctuations
  • reduced water hammer and vibrations
  • operating conditions closer to the best efficiency point
  • tangible benefits in terms of reliability and maintenance

hydrovar® X: integrated intelligence in Lowara pumping solutions

In Lowara pumping solutions, speed regulation represents much more than a tool for improving energy efficiency. Thanks to hydrovar X technology, the pump continuously adapts its performance to the actual needs of the building, limiting operational fluctuations that can result in noise, vibrations, and stress on piping systems.

The benefits are particularly evident in applications such as hotels, residential buildings, offices, and healthcare facilities, where water systems are located close to occupied environments. More stable pressure contributes to smoother system operation and reduces the phenomena that can propagate through pipes and building structures.

From a management standpoint, smoother operation also helps reduce component wear and improve service continuity over time. In addition, integration with Building Management Systems enables constant monitoring of system performance and early identification of anomalies before they affect operation.

“When discussing acoustic comfort in buildings, attention immediately goes to walls, materials, and insulation. In reality, the behavior of the hydronic system can also have a major impact on indoor environmental quality. A pump that continuously adapts to the actual demand of the building operates more steadily and helps reduce the phenomena that are often at the origin of noise and vibrations. This is precisely the approach behind Lowara solutions equipped with hydrovar X technology, which are increasingly requested in hotel, residential, and office projects where comfort, energy efficiency, and reliability are closely interconnected.”
Marco Dola, Product Manager, Booster Sets and HVAC Pumps, AW, Xylem

Whether for new installations or revamping projects, Lowara solutions equipped with hydrovar X technology therefore help improve occupant well-being by combining energy efficiency with quieter, more stable, and controlled operation.

Acoustic comfort is a design requirement, not a detail

In modern building design, energy efficiency, reliability, and acoustic comfort are increasingly interconnected aspects. Considering these factors from the earliest stages of system development helps prevent issues that are difficult and expensive to solve once the building is completed. In this context, Lowara solutions with hydrovar X technology provide a practical way to combine system performance with occupant well-being.

Would you like to learn more about how hydrovar X can be integrated into your project? Contact the Lowara technical team for a customized assessment of your installation.