Det ser ut som du kommer fra United States, men det aktuelle nettstedet du har valgt å besøke er Norway. Vil du endre nettsted?

Ja, takk! Nei, jeg vil være på det nåværende nettstedet

System Syzer

SYSTEM SYZER PSYCHROMETRY

Bell & Gossett is pleased to announce a new PC Application: System Syzer -Psychrometry

Sytem-Syzer_ 3.png

This new System Syzer tool is handy for design engineering that need to solve for a variety of questions surrounding the coil cooling process.

Features include:

  • Cooling process is graphed on the chart and animated to show the heat transfer direction
  • Calculates multiple psychometric characteristics based on two inputs
  • Calculates mass flow and cooling load (BTU)
  • Built-in design day temperature/humidity for 100 U.S. cities
  • Determines condensate rate of the coil
  • Show real time outdoor air conditions by inputting a weather site XML address

The application is free of charge and can be downloaded here

SYSTEM SYZER MOBILE

Bell & Gossett is pleased to announce the release of an iPad® and iPhone®and Android® version of its very popular System Syzer® Calculatortool. The application is free of charge and can be downloaded from the iTunes App Store. or the Google Play Store

Sytem-Syzer-2.png

The tool is made up several different calculators:

  • There is a calculator to determine the friction loss and velocity through various pipe types & sizes based on your fluid conditions.
  • Use System Syzer to determine the relationship between fluid temperatures, system flow and heating/cooling load.
  • Included is a Cv tool that shows the relationship between Cv, flow and head. Again, this calculator accounts for fluid properties.
  • There is a Pipe Length/Pressure Drop tool that is handy with the other calculators to view the relationship between pipe length, friction loss and total head loss.
  • We have also bundled the Circuit Setter® / Triple Duty Valve calculator that is very useful for balance contractors. Use it during design to help predetermine valve settings and out in the field to determine flow through the valves based on pressure drop readings.

Xylem offers a wide selection of specialized tools and calculators like the pump curve calculator, sewage pump calculator, and more to assist engineers make vital decisions for projects.

CALCULATOR WHEELS

Pasted Graphic.png

Circuit Setter® Balance Valves Calculator
Order Circuit Setter Calculator Wheel from local representative

Pasted Graphic 1.png

System Syzer® Calculator displays Reynolds numbers, flow rates, relative roughness and friction factors. The balance section is preset with gauge data for Circuit Setters and Triple Duty Valves.
Order System Syzer Calculator Wheel from local representative

;