It looks like you are coming from United States, but the current site you have selected to visit is Bulgarian. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode
Singapore’s island resort gets modern wastewater management

Singapore’s island resort gets modern wastewater management

Singapore, an island city-state with over 5.6 million inhabitants residing on a small land area of about 710 km2, has a water demand of about 430 million gallons a day. In order to meet its water management needs, Singapore has to develop innovative solutions to collect, treat, and reuse sewage and rainwater from all across the nation, including Singapore’s island resort of Sentosa.
 
Managed by Sentosa Development Corporation (SDC), Sentosa is home to an exciting array of themed attractions, lush rainforests, golden sandy beaches, luxury residences, and world-renowned golf courses. Collectively, this patch of paradise welcomed an impressive total of 19.1 million guests in 2017 and 2018.
 
Running a myriad of developments on a 500-hectare island presents many challenges, such as ensuring a steady supply of water and electricity, as well as an efficient wastewater management system. With a high volume of visitors, the island resort depends on a complex system of pumping stations to help remove sewage on demand.

Building resilience: upgrading an aging pump system

Designed in the 1990s, Sentosa’s complex pumping system and its programmable logic controller (PLC) algorithm were no longer fully suited for its current application. SDC decided to conduct an in-depth study of all existing pumps and found that several pumps had to be overhauled. An upgrade to the entire system was necessary, so the SDC team set out to search for a more robust solution, including pumps that have had a proven track record.
 
“Other than confirming that our old pumps could no longer fulfill our sewage disposal needs, the study also helped us realize that a monitoring system capable of generating incident reports would allow us to identify specific reasons for the pump breakdowns,” says Steven Kong, Senior Project Engineer, SDC.
 
The absence of a monitoring controller in the pumping system proved to be crippling to the pumping stations, as damaged pumps would go undiscovered. When they were finally identified, it was often too late. The broken pumps were mostly beyond repair and needed to be replaced completely.

New pumps, transmitters and monitoring systems

Following a thorough review, SDC decided to install three of Xylem’s solutions: Flygt N-pumps, MJK Shuttle® Ultrasonic level transmitters, and the Flygt MultiSmart® monitoring and control system. By pairing Flygt N-pumps with a trouble-free level transmitter and an intelligent pump station manager, Xylem’s solution addressed the island resort’s needs and eliminated its previous challenges.
 
Suitable for a broad range of wastewater applications, the N-pumps replaced the older pumps in 11 pumping stations across the southern region of Sentosa, with two units for dry well installation and nine units for wet well installation. Built with the patented N-technology comprising an innovative self-cleaning impeller, Flygt N-pumps helped lower SDC’s energy bills and reduce unplanned maintenance costs.
 
“The 11 pumping stations serve major tourist attractions, golf clubs and hotels,” says Kong. “The new pumps are still running with no clogging issues! We used to call-out vacuum trucks for scum removal once a month, but we haven’t needed that service since the installation of the Flygt N-pumps.”

Advanced remote monitoring capabilities

However, SDC still required a monitoring controller to pull the system together. With Xylem’s recommendation, the SDC team decided to install a scalable system with advanced remote monitoring capabilities for regular checks on the health of the system, providing adequate reaction time before any detrimental issues might surface.
 
“We used to struggle with the old pumping stations’ PLC program, whereas the MultiSmart® handles all basic and advanced functionalities on its own,” says Kong. “Furthermore, the controller’s history log was crucial in helping us identify the root cause of a flash flood that happened in one of the pumping stations a while back. With the logged in-depth events data, we had the information we needed to rectify the problem in a timely manner.”
 
The controller also boasts auto-reset capabilities for non-critical alarms, enhanced motor protection, and SMS messaging alerts.
 
“The SMS messaging alert system is by far our team’s favorite feature,” says Kong. “Problems with pumping stations can occur at any time of the day, and we don’t have personnel stationed near each station all the time. With the SMS messaging alerts, if a problem occurs, we’ll immediately receive a specific alarm notification, and can then address that problem promptly.”
 
Koh Chong Hin, Managing Director, Xylem Southeast Asia added, “Selecting the perfect technology for each application is crucial for achieving better water management. We’re glad that our solutions met Sentosa’s needs, and they haven’t experienced any major breakdowns since then. Most importantly, our solutions ensure Sentosa a smooth, reliable and low-maintenance operation for many years to come.”


Additional sources:
Department of Statistics Singapore, Population and Population Structure
Public Utilities Board, Singapore Water Story
Sentosa Development Corporation, Annual Report 2017/18