It looks like you are coming from United States, but the current site you have selected to visit is Anguilla. Do you want to change site?

Yes, please! No, keep me on the current site

Tackling water quality challenges for small pools

Efficient filtration solutions for small pools that improve water quality, reduce costs, and enhance safety

Filtration Pools & Leisure Attractions Aquatics Commercial Aquatic FIltration

Standing poolside at a swim school, health club, hydrotherapy center, splash pad or community center, what is the first thing you notice? The quality, color and clarity of the water. For smaller pools like these, the importance of filtration technology is just as critical as it is for larger commercial pools. Is it time to take responsibility and control for your pool safety? In this article, Scott Hyland, Aquatics Sales Director at Xylem, discusses the importance of filtration and how smaller pools can benefit from looking at alternative technologies.

While many are aware of the rigorous quality and safety standards required for large commercial pools, a safe and comfortable bather experience is just as important for smaller facilities. Regardless of pool size, filtration is critical to ensuring the hygiene of users and plays an important role in making the water look clean and inviting. 

Having high water quality and clarity is pleasant for users and encourages them to return, leading to greater customer retention and revenue. There are, however, many not-so-obvious benefits to maintaining high water quality through filtration. With crystal clear water, lifeguards and staff are able to see the bottom of the pool, essential to maintaining awareness and ensuring user safety. Likewise, removing contaminants like Cryptosporidium, a microscopic parasite, is essential to keep bathers safe and healthy. 

Traditionally, pools in the US have used sand filtration. Although these provide adequate filtration, they are large, use significant volumes of backwash water, and may require a flocculant to increase performance. An alternative to sand filters is pre-coat or regenerative media filters (RMF), in which a series of vertical elements are coated with a disposable filter medium, normally perlite. With far better filtration and no need for coagulants, RMF systems deliver chemical savings of up to 30%. 

Often an important consideration for smaller pools is the cost of filtration. Increasingly, we are seeing the use of renewable energy-powered systems in recreational facilities. Not only do these reduce the environmental footprint and associated emissions of running filtration systems, but they also reduce the energy bill and running costs of the facility by providing electricity for things like heating and lighting. Cost-saving and sustainable measures like this are becoming a focus of local authorities.  

With space and budget often limited for smaller aquatic facilities, Xylem has developed a cost-effective, space-saving, energy-efficient alternative filtration method. Based on Xylem’s industry-leading Neptune Benson Defender® RMF technology, the Defender® FP filter has been specifically designed for smaller pools with flows in the range of 107 - 300 gpm (24 - 68 m3/hr) and maintains optimum clarity and quality for the best possible bather experience. 

Thanks to its innovative design, the Defender FP filter does not require backwashing*. This helps to save money by reducing water waste while simultaneously eliminating the heating costs associated with heating make-up water. In fact, the average pool can realise savings of up to 90% water savings and up to 50% energy savings. Additionally, the superior turbidity reduction eliminates organics from the pool requiring less chemicals. 

Many aquatic facilities with small pools are restricted in their available space for filtration systems. The Defender FP filter is ideally suited to these conditions and is able to easily fit into smaller plant rooms due to its compact size. Easily retrofitted to existing spaces, the Defender FP filter is small enough to move through standard 36" doorways, eliminating the costly “knockdown and rebuild” approach too often required with larger sand filters. Once inside the plant room, the system’s small footprint frees up space for additional storage. 

If you are considering new filtration options for your aquatic facility, consider the compact, sustainable and cost-saving Neptune Benson Defender FP filter. With reduced lifetime ownership costs, better filtration and easy maintenance, this new system is ideal for small pools and is rapidly growing in popularity across the US.  

*Water is discharged to sewer/drain during perlite media replacement