Documents
-
Kraft Foods achieves excellent nutrient removals
Due to an expansion in potato chip production, the snack food plant required additional wastewater treatment capacity. It needed to be able to meet strict discharge limits for biochemical oxygen demand (BOD), total suspended solids (TSS), ammonia nitrogen (NH3-N), total nitrogen (TN), and total phosphorus (TP) regulations.
-
Landfill leachate treatment system significantly reduces operations cost
The South Central Counties Solid Waste Agency, located in Hopewell, Pennsylvania needed a cost effective, on-site treatment system to treat 12,500 gpd of leachate and allow for future expansion.
-
-
-
Logan Township, NJ expands water reclamation facility
Situated on the banks of the Delaware River, Logan Township, New Jersey has a long history of caring for its watershed and natural environment. In the early 70s, the town designed what has been described as “the nation’s first ecologically planned industrial complex,” Pureland Industrial Complex.
-
Low-pressure UV system ensures reliable and sustainable service water supply
The Böseler Goldschmaus GmbH & Co. KG site features its own modern wastewater treatment plant (38,500 ECW). To always ensure high water quality, a reliable solution was sought to keep the proportion of microorganisms, viruses, and multi-resistant germs safely below the prescribed limits without the use of chemicals.
-
Manchester City: Efficient rainwater capture and reuse through data and analytics
Manchester City FC is using smart technology and rainwater reuse to reduce potable water use across its Etihad Campus. With help from Xylem’s data-driven platform, the club aims to optimize irrigation and achieve full stormwater reuse by 2026.
-
Meeting expanding water needs at Jefferson Hospital
AHN Jefferson Hospital is an award-winning healthcare facility that provides comprehensive inpatient and outpatient surgical services in western Pennsylvania. The hospital’s state-of-the-art-surgical suite features an advanced robotic system, which is controlled by the surgeon for minimally invasive surgery.
-
Midas® OCM eliminates odors associated with sewer collection system
In 2004, a major west coast city began construction of two new interceptor sewers. The 12 foot diameter intercept lines relieve hydraulic overloading, but also created a number of turbulent areas where nuisance odors adversely affected the local residential community. These odors were primarily H2S at concentration levels of up to 150 ppm, as well as volatile organic contaminants (VOCs).
-
Milton Sewer Authority reduces wastewater strength by 90%
Settled in 1771 and incorporated into a borough in 1817, Milton is home to approximately 7,000 people in Northumberland County, Pennsylvania, USA. The municipally-owned Milton Regional Sewer Authority (MRSA) serves many residential customers, but a large portion of the MRSA’s wastewater treatment plant's influent comes from the manufacturing facilities of ConAgra Foods, the food giant that produces Chef Boyardee, Healthy Choice, Andy Capp, LaChoy, and Gulden’s Mustard products.
-
MiPro eco3 Advanced Oxidation Process for Taste and Odor Removal
After installing Xylem's Wedeco MiPro eco3 advanced oxidation process system K-Water was able to eliminate taste and odor complaints economically.
-
Mission-critical support: Xylem powers sewage reliability aboard the USS Hornet
To help address the USS Hornet’s urgent wastewater system needs, a Xylem Goulds Water Technology 1GD51G4AA model grinder pump was recommended to replace the damaged unit that serves one of the ship’s critical onboard sewage tanks. This support provided the museum with a reliable, high-quality replacement that restored confidence in an essential system while easing the financial burden on the nonprofit organization. -
Mixing It Up in Michigan
Before deciding on the 4320s, Kennedy Industries along with YCUA operations and maintenance personnel performed an extensive energy study of the aeration mixers.
-
Mobile equipment helps mining operation meet metal limits
In order to expand operations and maintain a water balance in South Carolina’s wet climate, Nevada Goldfields’ Barite Hills gold mining operation required a treatment plant to handle its wastewater. At this mining site, the company extracts gold from soil using a high pH cyanide leaching solution. The process generated large volumes of cyanide and metal laden wastewater, which they had been storing on-site.
-
-
-
Mobile water treatment eliminates iron level issues
This client operates a groundwater treatment facility at a Super Fund site where groundwater is pumped to a VOC stripper for the removal of TCE which is then re-injected into the aquifer. High iron levels in the groundwater caused fouling of pumps, pipes and well casings. This fouling threatened the reliability of the process in terms of flow.
-
-
MPW selects EnviroMix BioMix for upgrade at second plant
Read how Mount Pleasant Waterworks used EnviroMix BioMix™ technology at the Rifle Range Road WWTP to support plant expansion, optimize denitrification, and reduce O&M costs. -
-
-
Municipal drinking water treatment
Municipalities are often faced with VOC contamination of their source wells. Chemicals like Vinyl Chloride and Trichloroethylene can leach into aquifers used as source water for municipal wells. When this occurs, in many cases the most cost-effective solution is to treat the water to remove the VOCs using air stripping, which has been established as a Best Available Control Technology BACT for this application.
-
-