It looks like you are coming from United States, but the current site you have selected to visit is Armenia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Florida County Aims for Full Usage of Reclaimed Water

USA

Challenge
Hillsborough County has the largest retail reclaimed water program in the Nation, with more than 17,000 customers and agreements in place to serve another 5,000, for a total of 22,000 accounts. In 2009, the county produced about 34 million gallons per day on average, with over 22 million gallons being distributed to customers, while the rest was discharged into surface waters. The average annual use of reclaimed water was around 60 percent, a byproduct of Florida’s weather patterns. There were weeks every year when the utility was utilizing 100 percent of its reclaimed water and much less during the dry months and rainy season. The utility’s long-term goal was to achieve 100 percent beneficial use of its reclaimed water 365 days a year.

Solution
In July 2016, GE’s UF and reverse osmosis units and Xylem’s Wedeco MiPro™ portable trailer-based pilot plant was used for UV/peroxide advanced oxidation process (AOP) to produce potable reclaimed water at the Falkenburg WRF (Water Reclamation Facility). Tetra Tech–a provider of consulting, engineering, and technical services–collaborated with the WateReuse Association, Xylem, and GE to design, build, and operate the direct potable reuse pilot purification process to treat reclaimed effluent wastewater to comply with EPA drinking water standards.

Download Case study