It looks like you are coming from United States, but the current site you have selected to visit is Armenia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

RiverSurveyor 4.0: Collecting acoustic stationary and moving boat discharge data

Duration: 59:22

RiverSurveyor 4.0: The new standard in collecting acoustic stationary and moving boat discharge data You might have heard about some of the big upgrades to the powerful, multi-frequency RiverSurveyor-M9, but we didn’t want you to take our word for it – the proof is in the data – and we want to share examples on how RiverSurveyor 4.0 has dramatically simplified the data collection process for hydrologists and water monitoring specialists like you!

Join SonTek's Product Manager/Application Engineer Isaac Jones and Senior Hydrologist, Daniel Wagenaar as they highlight how RiverSurveyor 4.0 has improved work-flow processes for water monitoring agencies, such as the USBR and EC. They will also go over new features to include:

  • No tagline/tape measure required: With RiverSurveyor stationary live, automatically measure distance between stations with DGPS or RTK GPS equipped systems
  • Manual configuration: Now you can set blanking distance, cell size and number of cells for moving boat measurements
  • Real-time QA/QC warnings: Know when there could be a problem before there is one
  • Zipped files: New and improved compression and auto-decompression, providing faster access to large amounts of data
  • Sample filter: Remove your random velocity outliers with ease