It looks like you are coming from United States, but the current site you have selected to visit is Georgia. Do you want to change site?

Yes, please! No, keep me on the current site

Future-proofing data centres: How water-smart engineering unlocks energy efficiency and carbon reduction

As the global digital economy accelerates, data centres have become indispensable to modern life. Yet the same infrastructure that powers AI, cloud computing, and digital communications also consumes vast amounts of energy and water. With rising compute density, water scarcity concerns, and increasingly stringent sustainability regulations, the pressure on operators to reduce environmental impact has never been greater.

A growing body of evidence shows that the most significant and immediate opportunities for carbon reduction lie inside the mechanical systems that keep data centres running—specifically, cooling, pumping, and water‑management infrastructure. When designed intelligently, these systems create a pathway to meaningful, measurable reductions in both operational and lifecycle emissions.

Xylem, a global leader in water technology, is at the forefront of this transition. “Through a combination of high‑efficiency equipment, adaptive controls, and digital intelligence, Xylem helps operators rethink water‑system design not as an auxiliary function, but as a powerful decarbonisation lever.” says Igor Chodaton, International Business Development Manager.

The shifting landscape of data centre sustainability

Several macro‑forces are reshaping how data centres approach energy and water:

AI and high‑density compute loads:
New workloads introduce large, fluctuating thermal loads and demand cooling systems that adapt instantly without driving up energy use.

Regulatory pressure and ESG scrutiny:
Power Usage Effectiveness (PUE) and Water Usage Effectiveness (WUE) expectations are tightening worldwide, directly influencing capital access and community acceptance.

Resource constraints:
In many regions, water scarcity and grid instability have become critical barriers to new facility development. Operators must demonstrate responsible stewardship of both energy and water.

Economic volatility:
Rising power costs and carbon pricing mechanisms mean inefficient systems are no longer just environmentally problematic—they are financially unsustainable.

Amid these pressures, one principle has become clear: efficiency is the most reliable and powerful decarbonisation tool available today.

“Every kilowatt avoided is an emission avoided—for the entire lifetime of the facility.”

Why water‑system design matters more than ever

Cooling and pumping systems account for a significant portion of non‑IT energy consumption in most data centres. Their performance is determined long before a facility goes live—at the design and engineering stages.

Strategic decisions in hydraulics, pump selection, variable‑speed control, and water treatment can reduce energy use dramatically while safeguarding uptime. When combined with digital monitoring and analytics, these systems create a smart, adaptive environment that continuously drives down the energy and water footprint.

This shift—to seeing mechanical systems as strategic carbon assets—is where Xylem’s expertise becomes transformative.

Xylem’s integrated approach to low‑carbon water systems

With more than a century of brand heritage and a global footprint of engineering, service, and manufacturing locations, Xylem delivers end‑to‑end water‑system excellence built on three pillars: efficiency, adaptability, and intelligence.

  1. High‑efficiency pumping and adaptive control
    At the centre of Xylem’s efficiency strategy is the Hydrovar® X variable‑speed drive, featuring IE5 ultra‑premium motor technology and rare‑earth‑free design options. This platform dynamically matches pump output to system demand, reducing energy consumption by up to 40%.

    The Hydrovar® X ecosystem integrates seamlessly across multiple pump families—including vertical multistage, end‑suction, in‑line, and booster sets—making it suitable for both new builds and retrofits. Its modular, multi‑pump architecture ensures resilience and scalability as facilities expand.

  2. Real‑time intelligence through digital platforms
    Xylem Vue, the company’s open and vendor‑agnostic digital platform, consolidates all sensor, pump, valve, and building management data into one unified environment. By enabling predictive maintenance, real‑time optimisation, and automated control adjustments, it ensures systems operate at peak efficiency long after commissioning.

    Complementing this is Xylem Vue Secure Connect, an IoT‑powered monitoring tool that provides trend analysis, remote alerts, and condition‑based recommendations—reducing site visits and mitigating performance drift.

  3. Smart water stewardship
    Heat‑exchange efficiency relies heavily on water quality and flow stability. Xylem provides solutions that optimise treatment, minimise blowdown, and use alternative water sources where appropriate. Real‑time leak detection, consumption monitoring, and precision setpoint control support improved WUE and reduced reliance on potable water.

A framework for low‑carbon design and operation

Operators aiming to future‑proof their data centres should consider the following strategic steps:

  1. Set carbon and water targets at the outset and treat them as engineering constraints.
  2. Right‑size pump and cooling systems based on dynamic load modelling, not static peaks.
  3. Prioritise part‑load efficiency, where most equipment spends the majority of its runtime.
  4. Embed digital monitoring from day one to ensure long‑term optimisation.
  5. Adopt modular, upgrade‑friendly architectures to accommodate future compute and cooling needs.
  6. Implement continuous commissioning to maintain performance as operating conditions evolve.

This approach ensures that efficiency gains remain durable—not just at handover, but across decades of operation.

The business case: Lower cost, lower risk, higher confidence

Beyond environmental benefits, intelligent water‑system design provides compelling financial returns:

  • Energy savings deliver rapid payback—often within three years for retrofit applications.
  • Improved reliability reduces downtime risk and associated revenue loss.
  • Regulatory compliance becomes easier through automated reporting and verifiable performance data.
  • Deferred capital expenditure becomes possible when optimised systems stretch the useful life of existing assets.

In short, sustainability becomes a competitive advantage—not a compromise.

Conclusion: Water‑smart cooling as a competitive differentiator

The systems designed and deployed today will determine the environmental and economic performance of data centres for the next 20 to 30 years. As workloads intensify and resource pressures increase, operators must embrace efficiency, intelligence, and adaptability as foundational design principles.

Xylem’s integrated approach—combining high‑efficiency technologies, digital intelligence, and deep engineering expertise—offers a clear pathway to lower carbon, lower cost, and higher operational resilience.

Future‑proofing data centres begins with water. And with Xylem, that future becomes both sustainable and achievable.

"Through a combination of high‑efficiency equipment, adaptive controls, and digital intelligence, Xylem helps operators rethink water‑system design not as an auxiliary function, but as a powerful decarbonisation lever.”
Igor Chodaton, International Business Development Manager