It looks like you are coming from United States, but the current site you have selected to visit is Guyana. Do you want to change site?

Yes, please! No, keep me on the current site

Xylem pump cuts energy use by 50 percent at London’s Heathrow Airport cargo center pumping station

November 20, 2013

WHITE PLAINS, N.Y.--(BUSINESS WIRE)--Nov. 20, 2013-- Xylem Inc. (NYSE:XYL), a leading global water technology company focused on addressing the world’s most challenging water issues, has improved the efficiency of a wastewater pumping station at Heathrow Airport’s cargo center. According to a comparison study conducted by Heathrow Airport’s Water Services Department, the installation of Xylem’s Flygt Experior® wastewater pumping system has reduced the station’s energy consumption by half and also eliminated the need for maintenance call-outs since its installation in January 2013.

Heathrow Airport commissioned Xylem to evaluate the airport’s wastewater pumping system in the cargo center area of the airport which hosts heavy traffic and non-stop activity on a daily basis. Following the evaluation, Xylem was charged with developing and implementing a reliable and energy-saving wastewater pumping solution.

“With operations running so regularly, it is critical to ensure that systems are run in the most efficient way possible,” said Ian Jolly, director of Heathrow Airport’s Water Services Department. “As one of the world’s largest and busiest airports, with almost 70 million people travelling through our terminals in 2012, Heathrow is committed to working with innovative, reliable technology to cater for this consistently high passenger traffic.”

Xylem installed two Flygt Experior pumps featuring non-clog technology and two SmartRun™ intelligent pump controllers which monitor the specific energy use of the pumps and continually adjust the pump speed to ensure that the minimum amount of energy is being used for all cycles.

About Xylem

Xylem (XYL) is a leading global water technology provider, enabling customers to transport, treat, test and efficiently use water in public utility, residential and commercial building services, industrial and agricultural settings. The company does business in more than 150 countries through a number of market-leading product brands, and its people bring broad applications expertise with a strong focus on finding local solutions to the world’s most challenging water and wastewater problems. Xylem is headquartered in White Plains, N.Y., with 2012 revenues of $3.8 billion and approximately 12,900 employees worldwide. Xylem was named to the Dow Jones Sustainability World Index for the last two years for advancing sustainable business practices and solutions worldwide.

The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit us at www.xyleminc.com.

Source: Xylem Inc.

Xylem Inc.
Jennifer Jacob, +1-914-323-5745
Jennifer.Jacob@xyleminc.com

Xylem