It looks like you are coming from United States, but the current site you have selected to visit is Iraq. Do you want to change site?

Yes, please! No, keep me on the current site

Case Studies

Case Studies

  • Out-of-Round pipe emergency repair

    How Smith-Blair custom-engineered 624 MJ tapping sleeves solved a 5/8" out-of-round pipe challenge on aging ductile iron infrastructure in Florida.
  • Emergency sewer system repair

    40-year-old carbon steel pipe with catastrophic failure repaired in hazardous wet well conditions. Smith-Blair 675 restored system integrity with zero downtime.
  • Smith-Blair Bell Pack Stops Leaking Sewer Force Main in Miami

    The sewer force main was not just leaking into the streets but into the Intercoastal Waterways along the coast of Florida. Smith-Blair engineers developed the solution, sent drawings to the customer, got the drawings approved and then had fabrications team come in specifically to work on the 48 inch bell pack all night.
  • Smith-Blair Dismantling Joint Used In The Panama Canal

    The dismantling fitting will allow for easy removal and re-installation of the butterfly valve when valve maintenance is required. These fittings are part of the new Panamanian subway system pipeline relocation project that involves several thousand feet of pipeline.
  • Smith-Blair Flanged Coupling Adapter in Central Florida

    For this particular job, Smith-Blair built 36 inch Flanged Coupling Adapters (FCAs). The FCAs are designed to provide an efficient means to remove and reinstall the pumps, valves and other fittings during maintenance procedures.