It looks like you are coming from United States, but the current site you have selected to visit is Iraq. Do you want to change sites?

Yes, please. No. Keep me on the current site.

FAQs for Continuous Electrodeionization (CEDI)

Discover what CEDI has to offer for your water purification needs

Continuous Electrodeionization (CEDI) is a chemical-free, self-regenerating technology used to provide a consistent flow of high-quality deionized water.

With the growing costs of chemicals for regeneration and waste neutralization, and heightened safety concerns with handling hazardous chemicals, many industrial customers began seeking an alternative to cost-prohibitive, on-site regenerable ion exchange for creating ultrapure water. IONPURE®, an Evoqua brand, offers that solution. The first to commercialize CEDI in 1987, we have provided thousands of modules that deliver ultrapure water at capacities ranging from 0.013 m3/h (0.06 gpm) to 22.7 m3/h (100 gpm).

In short, CEDI is a water treatment process that uses a combination of ion-exchange resins, ion-exchange membranes, and direct current to continuously deionize water without the need for chemicals. The avoidance of chemicals helps to reduce the systems’ operating and maintenance costs and, therefore, improve your bottom line.

While both ion exchange and EDI use ion-exchange resins, the removal mechanisms are quite different. Conventional ion exchange utilizes chemically regenerated ion-exchange resins, which function in a capture (exhaustion cycle) and discharge (regeneration cycle) mode. This results in a breakthrough of ions at the end of the service cycle and a rinse out of regenerant at the beginning of the next service cycle. Capacity and selectivity are the most important resin properties in the mode of operation.

CEDI uses a reaction/transport mechanism to remove ions through resin under influence of a DC field. This requires a continuous path of like-charge resin beads. The transport is largely across the surface of the resin beads. Transport through resin bead (particle diffusion) can be limiting.

Some of the major advantages of CEDI over traditional mixed-bed deionization systems include:

No acid or caustic bulk storage, pumping, waste neutralization, or disposal issues
Lower operating costs due to lower manpower requirements, as well as lack of chemical regeneration

Power plants worldwide are switching out their conventional MBDI for IONPURE CEDI modules to feed boilers for steam generation. Designed similarly to reverse osmosis (RO) systems, they’re used in conjunction with RO as a polishing step for boiler feed water and cooling tower applications. For boilers, the modules provide deionized water to create the steam that turns the turbines.

Manufacturers of semiconductor devices need the highest in high purity water quality, requiring extremely low levels of contaminants such as sodium, silica, and boron. The microelectronics manufacturing industry also demands low maintenance technology that will operate efficiently with minimal downtime. Safety is also an industry concern, which is why more and more manufacturers are looking for a system that will reduce their chemical usage. Our CEDI modules are designed to deliver a continuous supply of uninterrupted ultra pure water with the added benefit of not using chemicals.

Did you know that most major multinational pharmaceutical companies use CEDI technology? The majority of the top 10 pharmaceutical companies own and operate multiple hot water sanitizable LX-HI units. The IONPURE LX CEDI modules are the only ones on the market that allow instantaneous hot water sanitization without temperature ramping, continuous operation at up to 60° C (140° F) and 2 bar/30 psi feed pressure during sanitization. There’s no need to re-torque these modules after installation/startup. IONPURE LX-X and LX-EU CEDI modules are also available for pharmaceutical applications where hot water sanitization is not required.

Our low-flow modules are used in laboratories, hospitals and universities for a wide range of applications, including:

  • Central water system for lab
  • Tabletop high-purity water systems for laboratory use
  • Feed to equipment such as autoclaves and clinical analyzers