It looks like you are coming from United States, but the current site you have selected to visit is Jordan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Blog Posts

Blog Posts

  • Blog Page

    Identifying and addressing the weak links

    Pure Technologies partnered with a southeastern U.S. utility to inspect a 24-inch potable water main in late 2015. The team inspected 9 miles (14 km) of the critical pipeline with the inline PipeDiver® platform.
  • Blog Page

    Thirty years of innovation in pipeline management

    Advances in technology and data analytics now enable utilities to manage pipelines through continuous, incremental investment rather than planning for end-of-life replacement. This approach reduces the overall cost of ownership by preventing failures and avoiding the unnecessary and disruptive replacement of assets with remaining service life.
  • Blog Page

    Leading the way

    More than a decade of pipeline inspection and monitoring positions Miami-Dade County as a leader in managing aging infrastructure.
  • Blog Page

    3 ways to protect your PCCP now and into the future

    Obtaining actionable condition insights helps utilities prevent sudden and high-consequence PCCP failures. But is your asset management plan equipped to prevent tomorrow’s failures? Explore three ways you can ensure PCCP assets operate safely over the long term.
  • Blog Page

    How to harness the power of your condition data

    Collecting condition data is critical for proactive pipeline management. Being able to make effective decisions on that data is just as important. Learn how advanced structural analysis helps utilities get more out of their inspection data.
  • Blog Page

    PCCP is never too young (or old) for a check up

    Prestressed Concrete Cylinder Pipe (PCCP) is the most inspected pipe in the world, with a proven track record of very low distress rates in most cases. Despite its reliable performance, just one bad pipe section can result in a pipeline failure.
  • Blog Page

    How large a leak could you be missing with CPM?

    Computational pipeline monitoring (CPM) is legislated on most pipelines in North America. While these systems are crucial in maintaining the integrity of a pipeline, they only operate at roughly 2-3% of throughput, and have a theoretical limit of 1% of throughput due to the error tolerance for meters.
  • Blog Page

    Wachs large valve solutions deliver big savings for utilities

    A utility client in the upper Midwest operates and maintains approximately 1,250 miles of water main, 31,000 system valves, approximately 1,320 large system valves (16” and larger) and has a maximum day demand of approximately 75 MGD.
  • Blog Page

    Asset management begins with leak detection

    A proactive leak detection strategy plays an important role in any asset management program. It allows utilities to obtain the general condition of their mains, since a leak not only represents a real water loss, but can also indicate the potential for pipeline failure.
  • Blog Page

    Establish system control and reliability

    The operability of critical valves is essential to control a water system and ensure system reliability. Critical valves control vital water transmission lines – the backbone of any water system. Operable critical valves reduce the consequences when large diameter pipeline failures occur.
  • Blog Page

    How to exceed standards in your Direct Assessment Program

    Despite its high strength, steel has a propensity to dent, buckle, corrode or crack when exposed, all risks to the integrity of a pipeline. In order to identify defects, proactive pipeline inspections are necessary to avoid failures, leaks or ruptures. One way of validating pipeline integrity is the use of Direct Assessment.
  • Blog Page

    Optimized valve maintenance – where to start

    When valves are not accessible or operable, crews have to back up and close more valves to isolate the line. It takes longer to complete the repair, more customers are impacted and potential of damage to property as a result of a main break increases.
  • Blog Page

    Where do you stand?

    Each day, 850 main breaks occur in North America. A study by Utah State University reported that the average break rate per 100 miles of pipe can be as high as 24.4 breaks per 100 miles of pipe.
  • Blog Page

    Usable field information that minimizes the consequence of failure

    Valve condition assessment services involve inspecting, operating, and assessing the mechanical condition and operational reliability of water main valves. Wachs Water Services provides a comprehensive condition assessment report detailing the operability of the asset including residual life, rehabilitation or repair.