-
Lliria Irrigation Association: comprehensive digitization of the irrigation system to improve operational efficiency and resilience
The implementation of an integrated solution, based on the Xylem Vue platform, has enabled the association to transition to digital, centralized, and real-time system management. -
Government of the Principality of Asturias: implementation of a DataHub for regional water cycle management
The solution was set up as a regional DataHub based on the Xylem Vue platform, and provides a comprehensive, centralized view of the regional water cycle to accelerate decision-making. -
CGUCJT: decision-support system for the Jucar-Turia Canal irrigation system
The implementation of Xylem Vue’s Agrotwin platform has enabled the CGUCJT to transition to digital, centralized, real-time management of the Jucar-Turia Canal’s main irrigation water delivery system. -
Brabant Water: end-to-end advanced water supply digitalization using Xylem Vue
Brabant Water deployed Xylem Vue to digitalize its network, integrating data for near real-time operational intelligence and non-revenue water management. -
Realtime monitoring cuts pollution risk at Scottish Water site
When a critical pumping station failed, Scottish Water used Xylem Vue Secure Connect monitoring and real-time data to restore resilience and protect the environment. -
ESAMUR: comprehensive digitalization platform for advanced monitoring of the wastewater treatment system in Murcia
The REGEN-IA project, built on the Xylem Vue platform, aims to integrate, govern, and leverage ESAMUR’s operational information within a single environment. -
Mimizan: reducing inflow and infiltration through centralized data collection and analysis
The Mimizan Federation of Municipalities is implementing the Xylem Vue platform to reduce inflow and infiltration by improving infrastructure monitoring. -
Redland city council: Cleveland WWTP operational improvement & data management project with Xylem Vue platform
Redland City Council unified plant operations data with Xylem Vue, boosting compliance monitoring and efficiency at Cleveland WWTP. -
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
ALJARAFESA: Advanced water cycle asset and work order management
Discover how ALJARAFESA modernized water cycle operations with a unified digital platform that connects asset management, maintenance, and leak detection to improve efficiency, responsiveness, and service delivery. -
Orekan (Navarre Regional Government): early warning system to reduce flood risk
The Autonomous Region of Navarre, located in northern Spain, has a surface area of over 10,000 km² and a population of approximately 680,000, concentrated mainly in the Pamplona metropolitan area. It has a highly complex hydrological system, as it is divided between the Ebro River basin, which covers approximately 90% of the region, and the Cantabrian basin, characterized by short, fast-responding basins. -
CABB: optimization of the primary wastewater network
The Bilbao Bizkaia Water Consortium (CABB) is the public utility responsible for managing the main drinking water and wastewater network in the province of Bizkaia, serving over one million residents through a range of water supply pipelines, sewer networks, and wastewater treatment plants across 97 municipalities. -
EMASESA: implementation of a digital twin to optimize decision-making in drinking water and wastewater management
Implementation of the Xylem Vue platform to optimize management, anticipate events, and improve the efficiency, resilience, and sustainability of the water cycle in Seville. -
EMASA: improving water efficiency through smart water balance analysis
EMASA (Empresa Municipal Aguas de Málaga S.A.) is the Malaga City Council’s public utility which has been in charge of managing the entire urban water cycle since 1987. The company serves more than 600,000 residents and supplies approximately 42 hm³ of drinking water. The system operates at a flow rate of up to 2 m³/s, ensuring urban water supply through an extensive pipeline network of around 2,000 km, divided into approximately 240 DMAs (District Metered Areas) and equipped with over 240,000 meters, 170,000 of which are smart devices. -
Gruppo CAP: intelligent water network management through advanced analytics and predictive asset planning
Gruppo CAP deployed Xylem Vue's AI-driven platform to optimize its 6,500 km water network, reducing water losses and improving asset management. -
Stadtentwässerung Celle: Wastewater treatment plant process optimization through artificial neural networks
Celle cuts energy consumption by 22% and chemical use by 56% using Xylem Vue WWTP optimization technology, saving tens of thousands of euros annually. -
CCACVI: Acquisition, implementation, hosting and maintenance of a hypervision solution for water and sanitation systems
The French Community of Communes Albères Côte Vermeille Illibéris (CCACVI) is promoting a hypervision project to streamline its water cycle, based on the Xylem Vue platform. -
ApaVital S.A.: Reduction of daily water losses by over 800 m³
ApaVital deploys Xylem Vue to reduce daily water losses by over 800 cubic meters, achieving compliance with EU regulations. -
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Eau d’Azur: France’s first smart water network cuts losses and strengthens drought resilience
The Metropolis of Nice is implementing a hypervision platform, based on Xylem Vue technology, to increase efficiency, sustainability, and resilience by providing a real-time view of the network. -
Scottish Water cuts energy by 60% with Flygt Concertor intelligent pump system
Scottish Water partnered with Xylem to upgrade hundreds of pumping stations with innovative, energy-efficient technology, as part of its commitment to reaching net-zero emissions. -
Herford utility: cutting CSOs by around 15% using an advanced prevention system
Inconsistent behavior and utilization of control structures was observed for past rainfall events. The municipality decided that an optimized network control system should be implemented to better utilize existing retention volumes, coordinate them effectively and reduce water pollution.
-
Hong Kong: development of digital twin pilot for trunk mains water systems in selected areas of New Territories East Region
This project aims to build and calibrate a hydraulic model for trunk mains water systems in selected areas of New Territories East Region and deploy the model through Idrica’s Real-Time What-If-Scenarios solution (now called Xylem Vue).