It looks like you are coming from United States, but the current site you have selected to visit is Kyrgyzstan. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Non-Genuine UV Lamp Replacement Compromises Performance and Water Treatment Reliability

Deciding to purchase a third party replacement part rather than the original manufacturer’s brand part is typically a matter of risk assessment. If deciding whether to purchase and install third party, non-genuine components that could potentially compromise the performance and reliability of a large-scale water disinfection operation, the risks can be quite high.

iStock-1265660329.jpgThis is what recently happened to a wastewater treatment plant situated in the Middle East region. A large Wedeco UV disinfection system was first installed and commissioned in 2008 and then expanded in 2017 to increase treatment capacity. The plant today has a design capacity of 25,792 cubic meters per hour (approximately 165 million gallons per day). During this 2017 expansion, the system owner opted to replace a portion of its original Wedeco Ecoray lamps with 3rd party non-genuine lamps. The decision to replace the Wedeco lamps was taken following a tendering process in which lowest pricing was the key influential factor in deciding which supplier secured the right to supply.

During this tender process, minimal consideration was taken into the potential effects, from a process performance or reliability perspective, of installing non-specification, non-genuine lamps into a Wedeco UV system.

Challenge

An increasing number of certification bodies, including NWRI and the USEPA’s UVDGM, require the use of original components in UV water disinfection systems to achieve compliance. But certifications and local compliance policies are different in different parts of the world, including the Middle East region. At this installation, replacement lamps were procured from an alternative supplier in Europe. The supplier of the non-genuine lamps was not offering any independent guarantees or validation in regards to the performance of the UV lamps they were supplying but they claimed their lamp is identical to the Wedeco Ecoray lamp, and that theirs would match or exceed the performance guaranteed by the Wedeco Ecoray lamps.

The UV system experienced immediate reliability issues upon removing the Wedeco lamps that had reached their end of life, and installing the non- genuine alternative lamps in their place.

The newly installed, non-genuine lamps were either failing or not performing adequately from the very early hours of the lamps projected life span.

As a result of installing non-genuine lamps, the end user experienced
a number of issues, including:

  • Significant increase in downtime due to failures
  • Increased maintenance costs, due to frequent lamp replacement
  • System reliability compromised
  • Inconsistency of UVC output from individual modules, due to having to mix individual lamp arrays with lamps having different run hours because of reliability issues
  • System disinfection performance and compliance challenges due to poor and inconsistent UVC output from the non-genuine lamps
  • Poor technical and process support from the non-genuine lamp supplier to help resolve reliability and performance problems during operational period
  • Eventually, the non-genuine 3rd parts lamps had to be removed from the system and new Wedeco Ecoray lamps were installed in their place

Solution

IMG_0817.jpg

During the six months of running non-genuine lamps, the end user recognized the original Wedeco lamps installed in other sections of the UV system continued to operate reliably and perform to the lamp’s guaranteed standards.

As a result of the challenges faced by the treatment process through the use of non-genuine lamps, Wedeco offered support and had fully qualified Wedeco Service Technicians perform Wedeco’s Condition Audit on the 3rd party lamps. The audit concluded, just as the end user also finally concluded, these non-genuine lamps were not equivalent in performance or reliability.

Results & Customer Benefits

With the Wedeco Ecoray lamps which have been installed, the system has not experienced any reliability or compliance issues. Only recommended routine maintenance was required to keep the system fully functional and performing to as-commissioned standards. The use of non-genuine lamps was intended to save cost. Instead it turned into a troublesome and costly experiment. Eliminating the non-genuine 3rd party lamps from the system, took it back to reliable operation.