Xylem Vue Secure Connect: Create a station with TCP XAM 912
Go through the set up wizard to create a station with Nexicon XAM 912 TCP modbus communication. As well how to change the IP address on the CCD 401 Gateway in the set up wizard.
It looks like you are coming from United States, but the current site you have selected to visit is Kyrgyzstan. Do you want to change site?
Go through the set up wizard to create a station with Nexicon XAM 912 TCP modbus communication. As well how to change the IP address on the CCD 401 Gateway in the set up wizard.