It looks like you are coming from United States, but the current site you have selected to visit is Lebanon. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode
< View all Making Connections
Disaggregation Tools and Trends for Utilities and What They Mean for AMI Next

Disaggregation Tools and Trends for Utilities and What They Mean for AMI Next

The energy industry is in the midst of a transformation, with exciting upgrades paving the way for smarter, more intelligent grid systems. Companies are improving their advanced metering infrastructure (AMI) capabilities and stepping into the era of “AMI Next." This next-generation approach prioritizes precision, agility, and data-driven innovations to meet growing energy demands while accommodating modern challenges like the increased adoption of electric vehicles (EVs), renewable energy integration, and customer-centric operations.

AMI 2.0 is supercharged by disaggregation tools, unlocking granular insights by breaking down energy consumption into individual components, such as EV charging sessions, HVAC systems, and other specific household or commercial loads. But what are the major trends in disaggregation tools, and how will they shape the future of utilities?

The Evolution of Disaggregation Tools

1. AI-Powered Insights

Artificial intelligence (AI) is revolutionizing how utilities approach disaggregation. Through machine learning algorithms, utilities can now parse through complex datasets and identify load signatures with remarkable precision. For example, AI tools can differentiate an EV's charging cycle from a refrigerator compressor, enabling utilities to pinpoint high-energy usage patterns in real time.

These AI-driven insights are also becoming more actionable. Utilities can use them to fine-tune demand response programs, create personalized customer incentives, and optimize overall grid performance. This dynamic level of intelligence marks a significant leap from traditional AMI systems, which primarily focused on total consumption without dividing it into specific uses.

2. Edge Computing for Greater Visibility and Control

Another trend in disaggregation tools is the shift toward edge computing. Unlike centralized cloud systems, edge devices process data locally at the point of measurement, such as on smart meters. Advanced meters, like the Stratus IQ+® from Sensus, are equipped with the computing power required for high-frequency data sampling and immediate analytics.

This real-time processing capability is critical for applications like EV charging management or outage mitigation, where latency can disrupt operations. With edge computing, utilities can react more swiftly, reducing both risks and costs associated with delays.

3. Integration with Distributed Energy Resources

With the rise of distributed energy resources (DERs), such as rooftop solar panels and battery storage systems, disaggregation tools are evolving to integrate these assets seamlessly into grid operations. Modern tools now provide insights into how DERs interact with traditional loads, helping utilities maintain balance and reliability.

For example, disaggregation combined with DER data can ensure that solar inverters and EV charging stations work in harmony, preventing overloads while maximizing efficiency. This trend aligns perfectly with the enhanced interoperability promised by AMI 2.0.

4. Customer-Focused Applications

Today’s energy consumers demand more transparency and control over their usage. Disaggregation tools are providing utilities with the means to deliver tailored experiences by offering customers breakdowns of their energy use. Utilities can now design apps or portals presenting homeowners with detailed insights into what appliances are using the most power, along with tips to reduce consumption.

Customer-facing initiatives not only promote energy efficiency but also enhance customer satisfaction, strengthening the relationship between utilities and their clients.

5. Enhanced Security and Privacy Protocols

With AMI 2.0 capable of generating unprecedented volumes of data, the question of cybersecurity becomes critical. Disaggregation tools are now being designed with advanced encryption and privacy compliance measures to safeguard sensitive customer information. This approach is essential as utilities expand their data collection and analysis capabilities while adhering to evolving regulatory requirements.

The Benefits of Disaggregation Tools in an AMI 2.0 World

Fully unlocking the potential of AMI 2.0 starts with putting customers at the center of utility operations. Disaggregation tools empower utilities to make smarter, data-driven decisions that directly address customer needs and elevate their experience in multiple ways.

1. Improved Load Management

Disaggregation tools provide utilities with precise data on when and where energy is consumed, right down to specific devices like EV chargers. With this detailed view, utilities can better balance supply and demand by identifying peak usage times, such as when EVs are most likely to charge. This foresight allows operators to shift peak loads, minimizing bottlenecks and optimizing power distribution. For customers, this translates to more reliable service and fewer interruptions, even as EV adoption grows. Encouraging off-peak charging via strategic messaging helps prevent grid strain while empowering users to make cost-efficient choices.

2. Strengthened Customer Engagement

Understanding consumption patterns on a granular level allows utilities to deliver tailored communications that resonate with customers. For example, disaggregated data can identify EV owners who may benefit from joining or adjusting their behavior within Time-of-Use (ToU) programs. Instead of generic reminders, utilities can offer specific suggestions like, "Shift your EV charging to save $50 per month," creating a positive and impactful experience. These personalized insights strengthen trust and promote energy-efficient habits, benefiting both utilities and their customers.

3. Enhanced Forecasting and Planning

Utilities rely on accurate data to make informed investments in infrastructure. Disaggregation tools shine here by pinpointing where future demand will grow, such as regions with high EV penetration or increased daytime solar usage. By identifying trends early, utilities can strategically expand infrastructure, adding EV charging stations or bolstering grid capacity exactly where it’s needed. These smarter investment decisions prevent wasted resources and ensure reliability, while customers benefit from well-prepared, future-ready services.

4. Cost Savings

Accurate, actionable data creates opportunities for utilities to save on operational costs. Disaggregation reduces the need for manual inspections and enables proactive maintenance, catching issues like overloaded transformers before they escalate. Additionally, by encouraging customers to adopt ToU programs, utilities avoid costly peak demand periods and achieve better overall grid efficiency. Customers, in turn, save money through lower energy costs by optimizing their usage in line with grid-friendly behaviors.

5. Enhanced Grid Reliability

With disaggregation tools monitoring energy usage at a micro level, utilities can quickly detect irregularities, such as failing equipment or imbalanced loads. By addressing these issues proactively, utilities prevent widespread outages, ensuring consistent and reliable service. For customers, this minimizes disruptions and reinforces trust in their utility provider as a reliable energy partner.

Preparing for the Future of Utilities with Disaggregation Tools

As your utility considers upgrading to AMI 2.0 or "AMI Next," the integration of advanced disaggregation tools should be a central focus. Here are key steps to prepare for this transition:

  1. Invest in Smart Meters with Edge Capabilities
     Deploy meters that not only measure consumption but also house the computational power to process and analyze data at the edge.
  2. Leverage AI and Machine Learning Solutions
     Partner with providers specializing in AI-based platforms that can continuously learn and adapt to evolving grid conditions.
  3. Prioritize Interoperability
     Ensure that new tools can integrate seamlessly with existing infrastructure, DERs, and future developments.
  4. Enhance Security Measures
     Invest in robust data protection frameworks to safeguard customer and operational data, aligning with regulatory standards.
  5. Educate Stakeholders
     Bring decision-makers, operators, and customers up to speed on the capabilities and benefits of disaggregation tools. Demonstrate the ROI through pilot projects or case studies.

Looking Ahead

The shift to AMI 2.0 is more than an upgrade; it’s a game-changer, driving smarter, more sustainable utility operations. Disaggregation tools, powered by AI and edge computing, are key to this evolution, enabling utilities to better understand energy use and build resilient, future-ready systems. Early adoption ensures a competitive edge, positioning utilities as leaders in the energy transition while delivering superior service to their communities. The future of utilities begins with AMI 2.0.

;