It looks like you are coming from United States, but the current site you have selected to visit is Lebanon. Do you want to change site?

Yes, please! No, keep me on the current site

Remote monitoring & controls for unmanned reliability

Long-term low volume seep collection

Challenge

Xylem was tasked with designing a seep collection system to collect water from a low volume seep through the wall of a decommissioned fly ash pond. The sump was located in an active river floodplain that flooded with as little as 1-2 inches of rain, so the customer needed an automatic shutdown when the river covered the sump. In addition, there was no existing power at this hard-to-reach location, so we had to provide the ability to remotely monitor and control the system.

“Custom control PLC panels provided the customer with a real time overview of performance variables as well as alarms...”

Solution

Xylem engineers developed an efficient, reliable system using Flygt submersible pumps and powered by Godwin generators. Custom control PLC panels provided the customer with a real time overview of performance variables as well as alarms, should the unmanned system encounter a problem.

Result

Backed by our extensive range of products and technical expertise, we met the project deadline while adapting to daily changes to the system design caused by intense regulatory pressure and state oversight. The system is still operational two years later and has required virtually no maintenance in that time. Thanks to our advanced telemetric monitoring and control capabilities, our customer has been able to minimize labor costs at this critical site while maximizing visibility and peace of mind.